Dear all
I am using one EVM430F6736 energy meter. I am having a issue with the power up process. Following steps have been followed by me.
1. I have connected 240V RMS at voltage terminals.
2. I have connected a current source at CUR terminals.
In manual it is mentioned that power up will be directly from HV source. No external voltage source is required for boosting the DSP. But it seems my EVM is not energized at all. Is there any indication that indicates the status of the EMV (Powered on or off).