Other Parts Discussed in Thread: DLPC3435
Greetings,
We are using the DLP LightCrafter Display 2010 evaluation model with the DLPC3435 display controller and the DLP2010 DMD. For a projection system we need to use the keystone correction to deal with distortion. It's writen in the user guide that the software can do keystone correction for up to +-40° angle. Now we are designing our system in Zemax and want to implement the keystone trapezoid.
So, my question is, how will the pre-distorted image look like on the DMD?
How should I set my field points in Zemax to simulate a keystone correction of let's say for example 40°?
How is the 40° angle related to the shape of the pre-distorted trapezoid?
Thank you very much for your help in advance.
Best regards
Frank