Hello,
whenever I connect my DLP LightCrafter 2000 to my 5V/2A power supply my EVM first turns LED D3 then LED D2 on, the projector starts flashing a red picture once, the EVM "reboots" and the same process happens over and over.
I assume it has to do with the little current provided by the 2A power supply, but 2A should work totally fine? Your manual says it needs at least 230mA to work properly...
I have to connect to power supplies in series in order to get the module somewhat working.
What can I do to get the module running?