Other Parts Discussed in Thread: DLPC3433, DLPC3478
Hi,
I would like to disable all the resize/crop/algorithm made on the input image of the lightcrafter.
My input image is in RGB 24 bits, format 1280x720 sent at 60 FPS. I would like to display them exactly wihout any modification from the lightcrafter. Image crop is set as following:
Start Pixel: 0
Start Line: 0
Pixels per line: 1280
Lines per frame: 720
However, I see black borders around my output display, which makes me think that my input image has actually been a little bit cropped to add these borders... Am I right ? Is there a way to get rid off these borders ? Is there any thing else I should disable/enable ?
Kind regards,
Julie