This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

MCSDK Video Demo



Hi,

    I want to run video MCSDK video demo on TDM6678l, I have tried to build the demo but there are warnings "No prep script found",

I checked for the same and got that its in cygwinxdc.bat file and there some path with are missing in it for active perl which are not available in my Active perl     setup. I have tried compiling it still and i got sv01.out file. i am trying to run it but its showing only loop back videos ie first row four videos only (checked for Firewall and antivirus also).

I go through readme.txt which form after make, which shows CPUTYPE as c6416 but i want it as shannon or c6678. So can you suggest anything for these problems or any sample code which will take video and transcode it and give it back to PC.

Thanks 

Tushar

  • Hi Tushar,

    For the real-time video demo, have you tried the pre-built image (sv01) included in MCSDK Video 2.0? Does that work with the instructions from the wiki page http://processors.wiki.ti.com/index.php/MCSDK_VIDEO_2.0_Demo_Guide? For your demo PC, does it have Giga-bit Ethernet card? Are you connecting your PC and the EVM with Giga-bit switch? Is ...\demos\demoroot\customBuild\tftp\sv0.out successfully loaded via TFTP? 

    To investigate the issue without video streaming from DSP, can you please provide us the complete log when running the following commands:

    1) run "genDemo.bat config.txt"

    2) run "sendPkts.bat"

    3) run "startMplayers.bat"

    4) run "ipconfig /all"

    CPUTYPE as c6416 in readme.txt is fine, and it is from our baseline code.

    If you would like to try video transcode without real-time requirements, MCSDK Video 2.0 provides a single-channel single-core H.264-H.264 transcode example in CCS project @ ...\mcsdk_video_2_0_0_10\examples\transcode. The data IO for this transcode example is via TFTP. To build this example, please have the patch as described in http://e2e.ti.com/support/dsp/c6000_multi-core_dsps/f/639/t/188748.aspx (3108.components.zip). A test clip can be found from http://e2e.ti.com/support/dsp/c6000_multi-core_dsps/f/639/p/177287/640766.aspx#640766 (airshow_p1280x720_4Mbps.zip).

    Thanks,

    Hongmei

  • Hi Tushar, a quick question which OS has your PC? Windows 7 or XP? .. Also, which Mplayer build are you using?

    thanks,

    Paula

     

     

  • Hi Hongmei,

     Thanks for replay....

    My log of run "genDemo.bat config.txt"


    2678.gendemo_debug.txt


     Log of run "sendPkts.bat"

    C:\Program Files\Texas Instruments\mcsdk_video_2_0_0_10\demos\demoroot>Reference\utils\bin\sendPackets.exe customBuild\config\autogen_config4sendPkts.cfg \Device\NPF_{0E682236-7FA0-48D2-811D-F0FA15A6DFFC} 100 s  
    
     config file: customBuild\config\autogen_config4sendPkts.cfg 
    
     adapter: \Device\NPF_{0E682236-7FA0-48D2-811D-F0FA15A6DFFC} 
    
     number of times, file to be replayed: 10161854 
    
    Read number of input files as : 3
    Attempting to send customBuild/cap/to_platform_merged24_4000pkts1.cap 
    
    
    Opened customBuild/cap/to_platform_merged24_4000pkts1.cap succesfully in offline mode
    Opened adapter succesfully in live mode to send packets out 
    Send queue allocated successfully 
    Sending packets loop 0 ..........
    packets from customBuild/cap/to_platform_merged24_4000pkts1.cap sent successfully 
    Attempting to send customBuild/cap/to_platform_merged24_4000pkts2.cap 
    
    
    Opened customBuild/cap/to_platform_merged24_4000pkts2.cap succesfully in offline mode
    Opened adapter succesfully in live mode to send packets out 
    Send queue allocated successfully 
    Sending packets loop 0 ..........
    packets from customBuild/cap/to_platform_merged24_4000pkts2.cap sent successfully 
    Attempting to send customBuild/cap/to_platform_merged24_4000pkts3.cap 
    
    
    Opened customBuild/cap/to_platform_merged24_4000pkts3.cap succesfully in offline mode
    Opened adapter succesfully in live mode to send packets out 
    Send queue allocated successfully 
    Sending packets loop 0 ..........
    packets from customBuild/cap/to_platform_merged24_4000pkts3.cap sent successfully 
    Number of times file played so far = 0 
    Attempting to send customBuild/cap/to_platform_merged24_4000pkts1.cap 
    
    
    Opened customBuild/cap/to_platform_merged24_4000pkts1.cap succesfully in offline mode
    Opened adapter succesfully in live mode to send packets out 
    Send queue allocated successfully 
    Sending packets loop 1 ..........
    packets from customBuild/cap/to_platform_merged24_4000pkts1.cap sent successfully 
    Attempting to send customBuild/cap/to_platform_merged24_4000pkts2.cap 
    
    
    Opened customBuild/cap/to_platform_merged24_4000pkts2.cap succesfully in offline mode
    Opened adapter succesfully in live mode to send packets out 
    Send queue allocated successfully 
    Sending packets loop 1 ..........
    packets from customBuild/cap/to_platform_merged24_4000pkts2.cap sent successfully 
    Attempting to send customBuild/cap/to_platform_merged24_4000pkts3.cap 
    
    
    Opened customBuild/cap/to_platform_merged24_4000pkts3.cap succesfully in offline mode
    Opened adapter succesfully in live mode to send packets out 
    Send queue allocated successfully 
    Sending packets loop 1 ..........
    packets from customBuild/cap/to_platform_merged24_4000pkts3.cap sent successfully 
    Number of times file played so far = 1 
    Attempting to send customBuild/cap/to_platform_merged24_4000pkts1.cap 
    
    
    Opened customBuild/cap/to_platform_merged24_4000pkts1.cap succesfully in offline mode
    Opened adapter succesfully in live mode to send packets out 
    Send queue allocated successfully 
    Sending packets loop 2 ..........
    packets from customBuild/cap/to_platform_merged24_4000pkts1.cap sent successfully 
    Attempting to send customBuild/cap/to_platform_merged24_4000pkts2.cap 
    
    
    Opened customBuild/cap/to_platform_merged24_4000pkts2.cap succesfully in offline mode
    Opened adapter succesfully in live mode to send packets out 
    Send queue allocated successfully 
    Sending packets loop 2 ..........
    packets from customBuild/cap/to_platform_merged24_4000pkts2.cap sent successfully 
    Attempting to send customBuild/cap/to_platform_merged24_4000pkts3.cap 
    
    
    Opened customBuild/cap/to_platform_merged24_4000pkts3.cap succesfully in offline mode
    Opened adapter succesfully in live mode to send packets out 
    Send queue allocated successfully 
    Sending packets loop 2 ..........
    packets from customBuild/cap/to_platform_merged24_4000pkts3.cap sent successfully 
    Number of times file played so far = 2 
    Attempting to send customBuild/cap/to_platform_merged24_4000pkts1.cap 
    
    
    Opened customBuild/cap/to_platform_merged24_4000pkts1.cap succesfully in offline mode
    Opened adapter succesfully in live mode to send packets out 
    Send queue allocated successfully 
    Sending packets loop 3 ..........
    packets from customBuild/cap/to_platform_merged24_4000pkts1.cap sent successfully 
    Attempting to send customBuild/cap/to_platform_merged24_4000pkts2.cap 
    
    
    Opened customBuild/cap/to_platform_merged24_4000pkts2.cap succesfully in offline mode
    Opened adapter succesfully in live mode to send packets out 
    Send queue allocated successfully 
    Sending packets loop 3 ..........
    packets from customBuild/cap/to_platform_merged24_4000pkts2.cap sent successfully 
    Attempting to send customBuild/cap/to_platform_merged24_4000pkts3.cap 
    
    
    Opened customBuild/cap/to_platform_merged24_4000pkts3.cap succesfully in offline mode
    Opened adapter succesfully in live mode to send packets out 
    Send queue allocated successfully 
    Sending packets loop 3 ..........
    packets from customBuild/cap/to_platform_merged24_4000pkts3.cap sent successfully 
    Number of times file played so far = 3 
    Attempting to send customBuild/cap/to_platform_merged24_4000pkts1.cap 
    
    
    Opened customBuild/cap/to_platform_merged24_4000pkts1.cap succesfully in offline mode
    Opened adapter succesfully in live mode to send packets out 
    Send queue allocated successfully 
    Sending packets loop 4 ..........
    packets from customBuild/cap/to_platform_merged24_4000pkts1.cap sent successfully 
    Attempting to send customBuild/cap/to_platform_merged24_4000pkts2.cap 
    
    
    Opened customBuild/cap/to_platform_merged24_4000pkts2.cap succesfully in offline mode
    Opened adapter succesfully in live mode to send packets out 
    Send queue allocated successfully 
    Sending packets loop 4 ..........
    packets from customBuild/cap/to_platform_merged24_4000pkts2.cap sent successfully 
    Attempting to send customBuild/cap/to_platform_merged24_4000pkts3.cap 
    
    
    Opened customBuild/cap/to_platform_merged24_4000pkts3.cap succesfully in offline mode
    Opened adapter succesfully in live mode to send packets out 
    Send queue allocated successfully 
    Sending packets loop 4 ..........
    packets from customBuild/cap/to_platform_merged24_4000pkts3.cap sent successfully 
    Number of times file played so far = 4 
    Attempting to send customBuild/cap/to_platform_merged24_4000pkts1.cap 
    
    
    Opened customBuild/cap/to_platform_merged24_4000pkts1.cap succesfully in offline mode
    Opened adapter succesfully in live mode to send packets out 
    Send queue allocated successfully 
    Sending packets loop 5 ..........
    packets from customBuild/cap/to_platform_merged24_4000pkts1.cap sent successfully 
    Attempting to send customBuild/cap/to_platform_merged24_4000pkts2.cap 
    
    
    Opened customBuild/cap/to_platform_merged24_4000pkts2.cap succesfully in offline mode
    Opened adapter succesfully in live mode to send packets out 
    Send queue allocated successfully 
    Sending packets loop 5 ..........
    packets from customBuild/cap/to_platform_merged24_4000pkts2.cap sent successfully 
    Attempting to send customBuild/cap/to_platform_merged24_4000pkts3.cap 
    
    
    Opened customBuild/cap/to_platform_merged24_4000pkts3.cap succesfully in offline mode
    Opened adapter succesfully in live mode to send packets out 
    Send queue allocated successfully 
    Sending packets loop 5 ..........
    packets from customBuild/cap/to_platform_merged24_4000pkts3.cap sent successfully 
    Number of times file played so far = 5 
    Attempting to send customBuild/cap/to_platform_merged24_4000pkts1.cap 
    
    
    Opened customBuild/cap/to_platform_merged24_4000pkts1.cap succesfully in offline mode
    Opened adapter succesfully in live mode to send packets out 
    Send queue allocated successfully 
    Sending packets loop 6 ..........
    packets from customBuild/cap/to_platform_merged24_4000pkts1.cap sent successfully 
    Attempting to send customBuild/cap/to_platform_merged24_4000pkts2.cap 
    
    
    Opened customBuild/cap/to_platform_merged24_4000pkts2.cap succesfully in offline mode
    Opened adapter succesfully in live mode to send packets out 
    Send queue allocated successfully 
    Sending packets loop 6 ..........
    packets from customBuild/cap/to_platform_merged24_4000pkts2.cap sent successfully 
    Attempting to send customBuild/cap/to_platform_merged24_4000pkts3.cap 
    
    
    Opened customBuild/cap/to_platform_merged24_4000pkts3.cap succesfully in offline mode
    Opened adapter succesfully in live mode to send packets out 
    Send queue allocated successfully 
    Sending packets loop 6 ..........
    packets fromTerminate batch job (Y/N)? Terminate batch job (Y/N)? 


    and 

    Log of run "startMplayers.bat"

    C:\Program Files\Texas Instruments\mcsdk_video_2_0_0_10\demos\demoroot>Reference\utils\bin\startMplayers.exe customBuild\config\subj-1080p-laptop.cfg 
    sdp://"C:\Program Files\Texas Instruments\mcsdk_video_2_0_0_10\demos\demoroot\Reference\config\demo1\sdp\t_rtp_1_0.sdp" -geometry 352x288+200+400 -fps 30 
    
    Mplayer 1 is Started 
    
    sdp://"C:\Program Files\Texas Instruments\mcsdk_video_2_0_0_10\demos\demoroot\Reference\config\demo1\sdp\t_rtp_1_1.sdp" -geometry 352x288+600+400 -fps 30 
    
    Mplayer 2 is Started 
    
    sdp://"C:\Program Files\Texas Instruments\mcsdk_video_2_0_0_10\demos\demoroot\Reference\config\demo1\sdp\t_rtp_1_2.sdp" -geometry 352x288+1000+400 -fps 30 
    
    Mplayer 3 is Started 
    
    sdp://"C:\Program Files\Texas Instruments\mcsdk_video_2_0_0_10\demos\demoroot\Reference\config\demo1\sdp\t_rtp_1_3.sdp" -geometry 352x288+1400+400 -fps 30
    
    Mplayer 4 is Started 
    
    sdp://"C:\Program Files\Texas Instruments\mcsdk_video_2_0_0_10\demos\demoroot\Reference\config\demo1\sdp\t_rtp_2_1.sdp" -geometry 176x144+200+750 -fps 30
    
    Mplayer 5 is Started 
    
    sdp://"C:\Program Files\Texas Instruments\mcsdk_video_2_0_0_10\demos\demoroot\Reference\config\demo1\sdp\t_rtp_2_3.sdp" -geometry 176x144+600+750 -fps 30
    
    Mplayer 6 is Started 
    
    sdp://"C:\Program Files\Texas Instruments\mcsdk_video_2_0_0_10\demos\demoroot\Reference\config\demo1\sdp\t_rtp_2_5.sdp" -geometry 176x144+1000+750 -fps 30
    
    Mplayer 7 is Started 
    
    sdp://"C:\Program Files\Texas Instruments\mcsdk_video_2_0_0_10\demos\demoroot\Reference\config\demo1\sdp\t_rtp_2_7.sdp" -geometry 176x144+1400+750 -fps 30
    
    Mplayer 8 is Started 
    
    sdp://"C:\Program Files\Texas Instruments\mcsdk_video_2_0_0_10\demos\demoroot\Reference\config\demo1\sdp\t_rtp_2_2.sdp" -geometry 176x144+380+750 -fps 30
    
    Mplayer 9 is Started 
    
    sdp://"C:\Program Files\Texas Instruments\mcsdk_video_2_0_0_10\demos\demoroot\Reference\config\demo1\sdp\t_rtp_2_4.sdp" -geometry 176x144+780+750 -fps 30
    
    Mplayer 10 is Started 
    
    sdp://"C:\Program Files\Texas Instruments\mcsdk_video_2_0_0_10\demos\demoroot\Reference\config\demo1\sdp\t_rtp_2_6.sdp" -geometry 176x144+1180+750 -fps 30
    
    Mplayer 11 is Started 
    
    sdp://"C:\Program Files\Texas Instruments\mcsdk_video_2_0_0_10\demos\demoroot\Reference\config\demo1\sdp\t_rtp_2_8.sdp" -geometry 176x144+1580+750 -fps 30
    
    Mplayer 12 is Started 
    
    sdp://"C:\Program Files\Texas Instruments\mcsdk_video_2_0_0_10\demos\demoroot\Reference\config\demo1\sdp\t_rtp_0_0_xp.sdp" -geometry 352x288+200+50 -fps 30
    
    Mplayer 13 is Started 
    
    sdp://"C:\Program Files\Texas Instruments\mcsdk_video_2_0_0_10\demos\demoroot\Reference\config\demo1\sdp\t_rtp_0_1_xp.sdp" -geometry 352x288+600+50 -fps 30
    
    Mplayer 14 is Started 
    
    sdp://"C:\Program Files\Texas Instruments\mcsdk_video_2_0_0_10\demos\demoroot\Reference\config\demo1\sdp\t_rtp_0_2_xp.sdp" -geometry 352x288+1000+50 -fps 30
    
    Mplayer 15 is Started 
    
    sdp://"C:\Program Files\Texas Instruments\mcsdk_video_2_0_0_10\demos\demoroot\Reference\config\demo1\sdp\t_rtp_0_3_xp.sdp" -geometry 352x288+1400+50 -fps 30
    
    Mplayer 16 is Started 
    
    sdp://"C:\Program Files\Texas Instruments\mcsdk_video_2_0_0_10\demos\demoroot\Reference\config\demo1\sdp\t_rtp_1_0.sdp" -geometry 352x288+200+400 -fps 30 
    
    Mplayer 1 is Re-started 
    
    sdp://"C:\Program Files\Texas Instruments\mcsdk_video_2_0_0_10\demos\demoroot\Reference\config\demo1\sdp\t_rtp_1_1.sdp" -geometry 352x288+600+400 -fps 30 
    
    Mplayer 2 is Re-started 
    
    sdp://"C:\Program Files\Texas Instruments\mcsdk_video_2_0_0_10\demos\demoroot\Reference\config\demo1\sdp\t_rtp_1_2.sdp" -geometry 352x288+1000+400 -fps 30 
    
    Mplayer 3 is Re-started 
    
    sdp://"C:\Program Files\Texas Instruments\mcsdk_video_2_0_0_10\demos\demoroot\Reference\config\demo1\sdp\t_rtp_1_3.sdp" -geometry 352x288+1400+400 -fps 30
    
    Mplayer 4 is Re-started 
    
    sdp://"C:\Program Files\Texas Instruments\mcsdk_video_2_0_0_10\demos\demoroot\Reference\config\demo1\sdp\t_rtp_2_1.sdp" -geometry 176x144+200+750 -fps 30
    
    Mplayer 5 is Re-started 
    
    sdp://"C:\Program Files\Texas Instruments\mcsdk_video_2_0_0_10\demos\demoroot\Reference\config\demo1\sdp\t_rtp_2_3.sdp" -geometry 176x144+600+750 -fps 30
    
    Mplayer 6 is Re-started 
    
    sdp://"C:\Program Files\Texas Instruments\mcsdk_video_2_0_0_10\demos\demoroot\Reference\config\demo1\sdp\t_rtp_2_5.sdp" -geometry 176x144+1000+750 -fps 30
    
    Mplayer 7 is Re-started 
    
    sdp://"C:\Program Files\Texas Instruments\mcsdk_video_2_0_0_10\demos\demoroot\Reference\config\demo1\sdp\t_rtp_2_7.sdp" -geometry 176x144+1400+750 -fps 30
    
    Mplayer 8 is Re-started 
    
    sdp://"C:\Program Files\Texas Instruments\mcsdk_video_2_0_0_10\demos\demoroot\Reference\config\demo1\sdp\t_rtp_2_2.sdp" -geometry 176x144+380+750 -fps 30
    
    Mplayer 9 is Re-started 
    
    sdp://"C:\Program Files\Texas Instruments\mcsdk_video_2_0_0_10\demos\demoroot\Reference\config\demo1\sdp\t_rtp_2_4.sdp" -geometry 176x144+780+750 -fps 30
    
    Mplayer 10 is Re-started 
    
    sdp://"C:\Program Files\Texas Instruments\mcsdk_video_2_0_0_10\demos\demoroot\Reference\config\demo1\sdp\t_rtp_2_6.sdp" -geometry 176x144+1180+750 -fps 30
    
    Mplayer 11 is Re-started 
    
    sdp://"C:\Program Files\Texas Instruments\mcsdk_video_2_0_0_10\demos\demoroot\Reference\config\demo1\sdp\t_rtp_2_8.sdp" -geometry 176x144+1580+750 -fps 30
    
    Mplayer 12 is Re-started 
    
    sdp://"C:\Program Files\Texas Instruments\mcsdk_video_2_0_0_10\demos\demoroot\Reference\config\demo1\sdp\t_rtp_0_0_xp.sdp" -geometry 352x288+200+50 -fps 30
    
    Mplayer 13 is Re-started 
    
    sdp://"C:\Program Files\Texas Instruments\mcsdk_video_2_0_0_10\demos\demoroot\Reference\config\demo1\sdp\t_rtp_0_1_xp.sdp" -geometry 352x288+600+50 -fps 30
    
    Mplayer 14 is Re-started 
    
    sdp://"C:\Program Files\Texas Instruments\mcsdk_video_2_0_0_10\demos\demoroot\Reference\config\demo1\sdp\t_rtp_0_2_xp.sdp" -geometry 352x288+1000+50 -fps 30
    
    Mplayer 15 is Re-started 
    
    sdp://"C:\Program Files\Texas Instruments\mcsdk_video_2_0_0_10\demos\demoroot\Reference\config\demo1\sdp\t_rtp_1_0.sdp" -geometry 352x288+200+400 -fps 30 
    
    Mplayer 1 is Re-started 
    
    sdp://"C:\Program Files\Texas Instruments\mcsdk_video_2_0_0_10\demos\demoroot\Reference\config\demo1\sdp\t_rtp_1_1.sdp" -geometry 352x288+600+400 -fps 30 
    
    Mplayer 2 is Re-started 
    
    sdp://"C:\Program Files\Texas Instruments\mcsdk_video_2_0_0_10\demos\demoroot\Reference\config\demo1\sdp\t_rtp_1_2.sdp" -geometry 352x288+1000+400 -fps 30 
    
    Mplayer 3 is Re-started 
    
    sdp://"C:\Program Files\Texas Instruments\mcsdk_video_2_0_0_10\demos\demoroot\Reference\config\demo1\sdp\t_rtp_1_3.sdp" -geometry 352x288+1400+400 -fps 30
    
    Mplayer 4 is Re-started 
    
    sdp://"C:\Program Files\Texas Instruments\mcsdk_video_2_0_0_10\demos\demoroot\Reference\config\demo1\sdp\t_rtp_2_1.sdp" -geometry 176x144+200+750 -fps 30
    
    Mplayer 5 is Re-started 
    
    sdp://"C:\Program Files\Texas Instruments\mcsdk_video_2_0_0_10\demos\demoroot\Reference\config\demo1\sdp\t_rtp_2_3.sdp" -geometry 176x144+600+750 -fps 30
    
    Mplayer 6 is Re-started 
    
    sdp://"C:\Program Files\Texas Instruments\mcsdk_video_2_0_0_10\demos\demoroot\Reference\config\demo1\sdp\t_rtp_0_3_xp.sdp" -geometry 352x288+1400+50 -fps 30
    
    Mplayer 16 is Re-started 
    
    sdp://"C:\Program Files\Texas Instruments\mcsdk_video_2_0_0_10\demos\demoroot\Reference\config\demo1\sdp\t_rtp_2_7.sdp" -geometry 176x144+1400+750 -fps 30
    
    Mplayer 8 is Re-started 
    
    sdp://"C:\Program Files\Texas Instruments\mcsdk_video_2_0_0_10\demos\demoroot\Reference\config\demo1\sdp\t_rtp_2_2.sdp" -geometry 176x144+380+750 -fps 30
    
    Mplayer 9 is Re-started 
    
    sdp://"C:\Program Files\Texas Instruments\mcsdk_video_2_0_0_10\demos\demoroot\Reference\config\demo1\sdp\t_rtp_2_5.sdp" -geometry 176x144+1000+750 -fps 30
    
    Mplayer 7 is Re-started 
    
    sdp://"C:\Program Files\Texas Instruments\mcsdk_video_2_0_0_10\demos\demoroot\Reference\config\demo1\sdp\t_rtp_0_0_xp.sdp" -geometry 352x288+200+50 -fps 30
    
    Mplayer 13 is Re-started 
    
    sdp://"C:\Program Files\Texas Instruments\mcsdk_video_2_0_0_10\demos\demoroot\Reference\config\demo1\sdp\t_rtp_1_0.sdp" -geometry 352x288+200+400 -fps 30 
    
    Mplayer 1 is Re-started 
    
    sdp://"C:\Program Files\Texas Instruments\mcsdk_video_2_0_0_10\demos\demoroot\Reference\config\demo1\sdp\t_rtp_1_1.sdp" -geometry 352x288+600+400 -fps 30 
    
    Mplayer 2 is Re-started 
    
    sdp://"C:\Program Files\Texas Instruments\mcsdk_video_2_0_0_10\demos\demoroot\Reference\config\demo1\sdp\t_rtp_1_2.sdp" -geometry 352x288+1000+400 -fps 30 
    
    Mplayer 3 is Re-started 
    
    sdp://"C:\Program Files\Texas Instruments\mcsdk_video_2_0_0_10\demos\demoroot\Reference\config\demo1\sdp\t_rtp_2_4.sdp" -geometry 176x144+780+750 -fps 30
    
    Mplayer 10 is Re-started 
    
    sdp://"C:\Program Files\Texas Instruments\mcsdk_video_2_0_0_10\demos\demoroot\Reference\config\demo1\sdp\t_rtp_2_6.sdp" -geometry 176x144+1180+750 -fps 30
    
    Mplayer 11 is Re-started 
    
    sdp://"C:\Program Files\Texas Instruments\mcsdk_video_2_0_0_10\demos\demoroot\Reference\config\demo1\sdp\t_rtp_2_5.sdp" -geometry 176x144+1000+750 -fps 30
    
    Mplayer 7 is Re-started 
    
    sdp://"C:\Program Files\Texas Instruments\mcsdk_video_2_0_0_10\demos\demoroot\Reference\config\demo1\sdp\t_rtp_0_1_xp.sdp" -geometry 352x288+600+50 -fps 30
    
    Mplayer 14 is Re-started 
    
    sdp://"C:\Program Files\Texas Instruments\mcsdk_video_2_0_0_10\demos\demoroot\Reference\config\demo1\sdp\t_rtp_0_2_xp.sdp" -geometry 352x288+1000+50 -fps 30
    
    Mplayer 15 is Re-started 
    
    sdp://"C:\Program Files\Texas Instruments\mcsdk_video_2_0_0_10\demos\demoroot\Reference\config\demo1\sdp\t_rtp_2_1.sdp" -geometry 176x144+200+750 -fps 30
    
    Mplayer 5 is Re-started 
    
    sdp://"C:\Program Files\Texas Instruments\mcsdk_video_2_0_0_10\demos\demoroot\Reference\config\demo1\sdp\t_rtp_2_7.sdp" -geometry 176x144+1400+750 -fps 30
    
    Mplayer 8 is Re-started 
    
    sdp://"C:\Program Files\Texas Instruments\mcsdk_video_2_0_0_10\demos\demoroot\Reference\config\demo1\sdp\t_rtp_0_3_xp.sdp" -geometry 352x288+1400+50 -fps 30
    
    Mplayer 16 is Re-started 
    
    sdp://"C:\Program Files\Texas Instruments\mcsdk_video_2_0_0_10\demos\demoroot\Reference\config\demo1\sdp\t_rtp_1_3.sdp" -geometry 352x288+1400+400 -fps 30
    
    Mplayer 4 is Re-started 
    
    sdp://"C:\Program Files\Texas Instruments\mcsdk_video_2_0_0_10\demos\demoroot\Reference\config\demo1\sdp\t_rtp_2_3.sdp" -geometry 176x144+600+750 -fps 30
    
    Mplayer 6 is Re-started 
    
    sdp://"C:\Program Files\Texas Instruments\mcsdk_video_2_0_0_10\demos\demoroot\Reference\config\demo1\sdp\t_rtp_2_2.sdp" -geometry 176x144+380+750 -fps 30
    
    Mplayer 9 is Re-started 
    
    sdp://"C:\Program Files\Texas Instruments\mcsdk_video_2_0_0_10\demos\demoroot\Reference\config\demo1\sdp\t_rtp_0_0_xp.sdp" -geometry 352x288+200+50 -fps 30
    
    Mplayer 13 is Re-started 
    
    Terminate batch job (Y/N)? 


    i have tried the video it shows only 4 windows of Mplayer which are Loop back videos....

    Please suggest me some solution....

    Thanks

    Tushar


    My Log of 

  • Hi Paula,

    I am Using XP and I dont know Mplayer version, I have download it from ti wiki link it is having name link this MPUI.2011-06-09.Light-Package.

    Thanks Tushar

  • Hi Tushar,

    I faced a similar issue, but cannot recall exactly how I fix it.. Two things that you can try are

    1) Reinstall Mplayer and select "Runtime CPU detection"

    2) Unistall 2011 and try 2008 (MPUI.2008-02-10.Full-Package.exe). If the second one is used please check as well "Runtime CPU detection"

    Also as Hongmei mentioned, please check that you are using a Gigabit switch or try to connect directly the board to you PC

    Thank you,

    Paula

     

  • HI,

    I try with MPUI.2008-02-10.Full-Package.exe but its still giving me only 4 videos which may be loop back video and i am using Ethernet switch. Can you suggest any other solution for this problem....


    Thanking you


    Regards

    Tushar

  • Hi Tushar,

    The logs you sent earlier look fine. Can you please do some basic checks? Can you please also provide the log for "ipconfig /all"?

    1) Are you using pre-built sv01.out (the file is located at demos\demoroot\Reference\sample_build)?

    2) What's the size of demos\demoroot\customBuild\tftp\sv01.out? With pre-built sample build, size of this generated custom build should be 21,827,161 bytes.

    3) Is the custom build (demos\demoroot\customBuild\tftp\sv01.out) correctly loaded through TFTP?

    4) Does your demo PC have Giga-bit Ethernet Card? The demo needs Giga-bit card.

    5) Please try direct connect between the EVM and your PC.

    6) If a laptop is used for the demo, please do not put it on a docking station.

    After the above checks, we can do the following:

    Use Wireshark to capture the packet flow between demo PC and DSP. IP of demo PC is 192.168.0.102. For Demo 1, core 0-5 are used and their IPs are 192.168.0.120-192.168.0.125, and their MACs are 0x0A,0x00,0x28,0x04,0xD5,0x4C to 0x0A,0x00,0x28,0x04,0xD5,0x51 (specified in demos\demoroot\Reference\config\demo1\demoCfg.pl). First check if demo PC is sending packets to the DSPs with correct IP and MAC addresses. If so, then check if there are packets coming from the DSPs. 

    Please let us know the results of the above checks. We can look more into it if there are still problems.

    Thanks,

    Hongmei

  • Hi Hongmei,

    I have tried all above things

    my ipconfig /all

    
    Windows IP Configuration
    
    
    
            Host Name . . . . . . . . . . . . : 32CBANSHULPC
    
            Primary Dns Suffix  . . . . . . . : EIC.COM
    
            Node Type . . . . . . . . . . . . : Unknown
    
            IP Routing Enabled. . . . . . . . : No
    
            WINS Proxy Enabled. . . . . . . . : No
    
    
    
    Ethernet adapter Local Area Connection:
    
    
    
            Connection-specific DNS Suffix  . : 
    
            Description . . . . . . . . . . . : Intel(R) PRO/100 VE Network Connection
    
            Physical Address. . . . . . . . . : 00-19-D1-46-27-A8
    
            Dhcp Enabled. . . . . . . . . . . : No
    
            IP Address. . . . . . . . . . . . : 192.168.0.102
    
            Subnet Mask . . . . . . . . . . . : 255.255.255.0
    
            Default Gateway . . . . . . . . . : 192.168.0.1
    
    

    my tftp log are

    Connection received from 192.168.0.126 on port 1234 [23/05 09:43:44.390]
    Read request for file <sv01.out>. Mode octet [23/05 09:43:44.406]
    Using local port 1090 [23/05 09:43:44.406]
    <sv01.out>: sent 42632 blks, 21827161 bytes in 10 s. 0 blk resent [23/05 09:43:54.265]

    1. i have tried using pre build sv01.out still having same problem, i can see only four videos on the screen.

    2. size of my prebuild demo is same as given by you. but the demo file given @ demos/demoroot/customebuild/tftp/sv01.out is 19,644 kb

    3. I think my custombuild is correctly loaded i have attached my tftp log please check it also.

    4. I have also tried by directly connecting EVM to PC still its having same problem.

    5. I checked Network packets on wireshark but its giving video source only my PC and i didnt got any packets from IP of DSp.

     I got correct IP and MAC address of all cores as mentioned.

    6. I have also tried it on another PC with Gb ethernet still i am having all above problems

      here i have attached ipconfig of that PC (Firewall is off)

    Windows IP Configuration
    
       Host Name . . . . . . . . . . . . : terminator
       Primary Dns Suffix  . . . . . . . : 
       Node Type . . . . . . . . . . . . : Hybrid
       IP Routing Enabled. . . . . . . . : No
       WINS Proxy Enabled. . . . . . . . : No
    
    Ethernet adapter Local Area Connection:
    
       Connection-specific DNS Suffix  . : 
       Description . . . . . . . . . . . : JMicron PCI Express Gigabit Ethernet Adapter
       Physical Address. . . . . . . . . : 00-90-F5-AB-FC-92
       DHCP Enabled. . . . . . . . . . . : No
       Autoconfiguration Enabled . . . . : Yes
       Link-local IPv6 Address . . . . . : fe80::4c39:bdd9:b9ac:e538%11(Preferred) 
       IPv4 Address. . . . . . . . . . . : 192.168.0.102(Preferred) 
       Subnet Mask . . . . . . . . . . . : 255.255.255.0
       Default Gateway . . . . . . . . . : 192.168.0.1
       DHCPv6 IAID . . . . . . . . . . . : 234918133
       DHCPv6 Client DUID. . . . . . . . : 00-01-00-01-17-25-E3-54-00-90-F5-AB-FC-92
       DNS Servers . . . . . . . . . . . : fec0:0:0:ffff::1%1
                                           fec0:0:0:ffff::2%1
                                           fec0:0:0:ffff::3%1
       NetBIOS over Tcpip. . . . . . . . : Enabled
    
    Tunnel adapter isatap.{92014E0A-37AF-4A63-8227-F50AB3D7D9DA}:
    
       Media State . . . . . . . . . . . : Media disconnected
       Connection-specific DNS Suffix  . : 
       Description . . . . . . . . . . . : Microsoft ISATAP Adapter
       Physical Address. . . . . . . . . : 00-00-00-00-00-00-00-E0
       DHCP Enabled. . . . . . . . . . . : No
       Autoconfiguration Enabled . . . . : Yes
    
    Tunnel adapter Teredo Tunneling Pseudo-Interface:
    
       Media State . . . . . . . . . . . : Media disconnected
       Connection-specific DNS Suffix  . : 
       Description . . . . . . . . . . . : Teredo Tunneling Pseudo-Interface
       Physical Address. . . . . . . . . : 00-00-00-00-00-00-00-E0
       DHCP Enabled. . . . . . . . . . . : No
       Autoconfiguration Enabled . . . . : Yes
    

    I am also not able to ping to the target, is there any provision to know that code is properly build on the Target and its working inside it....

    Waiting for your replay

    Thanking you...

    Regards

    Tushar

  • Hi Tushar,

    Which sv01.out are you loading from TFTP? Is it demos\demoroot\customBuild\tftp\sv01.out or something else?

    From your tftp log, I am seeing file size of 21827161 bytes. However, we should load demos\demoroot\customBuild\tftp\sv01.out, whose size should be 20,135,434 bytes, or 19,644 kb as you mentioned above.

    Also would like to clarify the use of pre-built and rebuilt sv01. In MCSDK Video 2.0 release package, pre-built sv01 is included under demos\demoroot\Reference\sample_build directory. In order to bring up a video demo on a particular demo PC, we need to patch the demo ID and MAC address of the demo PC into sv01. This is done by modifying config.txt and then running "genDemo.bat config.txt" from demos\demoroot. Running this batch file will generate customized sv01.out at demos\demoroot\customBuild\tftp, which is then loaded through TFTP for showing the demo on the demo PC.

    If a user re-compiles sv01, an updated sv01.out will show up at dsp\mkrel\sv01 directory. To use this recompiled sv01.out for video demo, it needs to be copied to demos\demoroot\Reference\sample_build directory. Then, rerun "genDemo.bat config.txt" to get an updated sv01.out at demos\demoroot\customBuild\tftp directory. After that, still load demos\demoroot\customBuild\tftp\sv01.out for the demo.

    A few more things we can check if you have CCS:

    1) Stop "sendPkts.bat " and "startMplayers.bat", and then connect to Core 0

    2) Load Symbols on Core 0: use demos\demoroot\customBuild\tftp\sv01.out

    3) Check if dsiuNwLocContext.numL4PktsSent increments or not (this can be done by running Core 0 for several seconds and then stop to check the value)

    4) If the above counter is incrementing, then sv01.out is correctly loaded and DSP is sending out RTCP packets. If so, GMAC Tx stats (i.e., value of register 0x2090C34) should increment also.

    5) If both 3) and 4) are good, Wireshark should be able to capture the RTCP packets from DSP if  PC and EVM are correctly connected (e.g., through a Ethernet cable).

    Thanks,

    Hongmei

  • Hi Hongmei,

    Thanx alot..

    I am able to run this video demo now, Actually i was using wrong .out file.

    Thanks

    Tushar P

  • could you share with me the MPUI.2008-02-10.Full-Package.exe?

    I didn't find it for several days.

    thx first.

  • Wang, we cannot upload .exe here, which kind of problem are you facing?

    thank you,

    Paula

  • my PC's OS is win7, can it  use MCSDK VIDEO?

    if can, but I meet a trouble,help me !

    it list in  http://e2e.ti.com/support/dsp/c6000_multi-core_dsps/f/639/p/879383/reply.aspx

    thank you !

  • Hi Lei, FYI, I tested SV01 Multicore transcoder demos (http://processors.wiki.ti.com/index.php/MCSDK_VIDEO_2.1_PKT_Demo_Guide) using MPUI.2011-06-09.Full-Package.exe (as well as MPUI.2008-02-10.Full-Package.exe) in a Windows 7 machine and they went ok.  let me know if you face any issue with PKT demos.

    thank you,

    Paula

  • hi, Paula

    I'd finish the sv01.out.

    but I have met a problem for a week. It lists in http://e2e.ti.com/support/dsp/c6000_multi-core_dsps/f/639/p/251383/879803.aspx#879803

    the TFTP cannot transport data or receive data, can you help me solve it.

    thank you

    lei. 

  • hi, Paula.

    I have complete the demo of sv04.out. now, I want to add my codec(AVS) into in project. I have reference this web(http://processors.wiki.ti.com/index.php/MCSDK_VIDEO_2.1_CODEC_TEST_FW_User_Guide), but I don't know how to build a lib. is it create a new project alone select "library not execute"? if so,  whether I should create a project to compile the source code which have complete the codec function in Visual Studio 2010. 

    another problem is post in the "http://e2e.ti.com/support/dsp/c6000_multi-core_dsps/f/639/t/253096.aspx"

    can you help me?

    thank you!