This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Periodical rise of CPU load



Hello,

I'm running video D1 capturing on DM365 under Linux (simple QBUF/DQBUF loop on v4l device, not through DMAI). The 'top' shows that the process takes about 0% of CPU load. But each 4.5 minutes CPU load of the process rises up to 25% for 3-5 seconds.

During test every possible non-related task or service are disabled.

When testing it on Kernels 2.6.18, 2.6.32, 2.6.37, we get the same results.

What can be the cause?

Thanks in advance.