This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

16bit LCD Interface modification using DM3730

Dear Members 

Q1) According to DM3730 Technical note, I understood that 18-bit Interface can't use look-up table and OSD Function. 

      12/16/24 bits I/F can use loo-up table. 

      Is that correct? 

     What is the function that DM3730 can't support under 18-bit interface conditions? ( as compared to 24bit and 16 bit interface) 

  Q2) According to logic-PD as attached ( It is very important for new pcb) 

(from attached file ) 

16-bit SOM Hardware Interface to 18-bit LCD Panel
Before the OS display driver can work, the microprocessor LCD controller must be connected correctly to the LCD color signals. In this example, we connect a 16-bit CPU hardware interface to an 18-bit LCD panel. The advantage of using 16-bit is that the software driver support is already available and does not cause the same loss of performance that may occur when supporting 18-bit display panels due to extra data being fetched across the memory bus. The extra low-order bits for red and blue on the LCD panel are simply driven with copies of the high order bits.

We will use the schematic as attached. 

Is that correct? 

0513.1020853B_AN502_LogicPD_DevKit_LVDS_Integration (1).pdf