This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

8148 EMAC



Hi,
We have a design based on the DM8148 and a BCM5461 Gigabit PHY.  we use RGMII mode in our design.
Our problem is that the ethernet interface appears to can not work in u-boot.  
in u-boot we use cmd ping
ping 10.33.0.69
link up on port 0, speed 100, full duplex
Using cpsw device
ping failed; host 10.33.0.69 is not alive
We think we have the PHY hooked up correctly .
Is there ang special seting for BCM5461. 

thanks

steve