This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

OMX Capture Encode

Other Parts Discussed in Thread: TVP7002

Capture encode is hanging on capture state execute

rago 2011.05 dm816x-evm ttyO2

dm816x-evm login: root
root@dm816x-evm:~# cd dm816x-evm/omx/
root@dm816x-evm:~/dm816x-evm/omx# ./capture_encode_a8host_debug.xv5T -o test.dat
a -m 1080p -f 60 -b 10000000 -n 500
output file: test.data
bit_rate: 10000000
frame_rate: 60
num_frames: 500
mode: 1080p
 Capture-Encode example
===============================
 OMX_Init completed
 UIAClient is ready to send a UIA configuration command
UIAClient received UIA_CONFIGURE_ACK
UIAClient is done sending requests
UIAClient is ready to send a UIA configuration command
UIAClient received UIA_CONFIGURE_ACK
UIAClient is done sending requests
 openeing file
 capture compoenent is created
 control TVP compoenent is created
Buffer Size computed: 3110400
set input port params (width = 1920, height = 1080)enable capture output port
got eventEnable/Disable Event
 dei compoenent is created
set input port params (width = 1920, height = 1080)
set output port params (width = 1920, height = 1080)set output port params (width = 1920, height = 1080)set number of channelsset input resolutionset output resolutionenable dei input port
got eventEnable/Disable Event
enable dei output port 0
got eventEnable/Disable Event
enable dei output port 1
got eventEnable/Disable Event
 encoder compoenent is created
found handle 0x123008 for component OMX.TI.VPSSM3.VFDC
 got display handle
found handle 0x126b10 for component OMX.TI.VPSSM3.CTRL.DC
Buffer Size computed: 4147200
set input port params (width = 1920, height = 1080)setting input and output memory type to defaultenable input port
got eventEnable/Disable Event
 connect call for capture-Dei
  connect call for dei- encoder
  connect call for dei-display
 got eventState changed to: OMX_StateIdle
 Capture outport buffers allocated
 got eventState changed to: OMX_StateIdle
 Capture is in IDLE state
 Dei input port use buffer done
  DEI outport buffers allocated
 got eventState changed to: OMX_StateIdle
 DEI is in IDLE state
 encoder input port use buffer done
  encoder outport buffers allocated
 got eventState changed to: OMX_StateIdle
 Encoder state IDLE
 got eventState changed to: OMX_StateIdle
 ctrl-dc state IDLE
  display buffers allocated
 waiting for IDLEgot eventState changed to: OMX_StateIdle
 display state IDLE
 got eventState changed to: OMX_StateExecuting
 display control state execute
 got eventState changed to: OMX_StateExecuting
 display state execute
 got eventState changed to: OMX_StateExecuting
 encoder state execute
 got eventState changed to: OMX_StateExecuting
 dei state execute
 got eventState changed to: OMX_StateExecuting
 capture state execute