This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DM8168 set the DDR CLK



hi ,

everyone

 who can tell me how to change the clock of the DDR3 in uboot on the evm board of  DM8168?
When I set the u-boot as flowers:

In arch/arm/include/asm/arch-ti81xx/clocks_ti816x.h which is in /ti-ezsdk_dm816x-evm_5_03_00_09/board support/u-boot-2010.06-psp04.00.01.13.patch1,

I add the #define shown below as appropriate
#define DDR_PLL_675 /* Values supported 400,531,675,796 */ 

In arch/arm/include/asm/arch-ti81xx/ddr_defs_ti816x.h which is in /ti-ezsdk_dm816x-evm_5_03_00_09/board support/u-boot-2010.06-psp04.00.01.13.patch1,

I add the #define shown below as appropriate

[...] 
#ifdef CONFIG_TI816X_EVM_DDR3
 #define CONFIG_TI816X_DDR3_675 /* Values supported 400,531,675,796 */ 
#define CONFIG_TI816X_DDR3_SW_LEVELING /* Enable software leveling as part of DDR3 init */ 
[...]
 
The Serial print "DDR clk: 675MHz " ,but actually t the measuring of the DDR CLK is  796MHZ usingoscilloscope,
and the value of the DDR PLL Control Registers is  corresponding to 796MHZ。

 
  • Hi Lingyi ying,

    Change macros at these two locations, then frequency will change to 675MHz.

    In arch/arm/include/asm/arch-ti81xx/ddr_defs.h file
    -#define CONFIG_TI816X_DDR3_796 /* Values supported 400,531,675,796 */
    +#define CONFIG_TI816X_DDR3_675 /* Values supported 400,531,675,796 */

    In arch/arm/include/asm/arch-ti81xx/clocks_ti816x.h file
    -#define DDR_PLL_796    /* Values supported 400,531,675,796 */
    +#define DDR_PLL_675    /* Values supported 400,531,675,796 */

    With the above two modification I had seen values changed in the DDR_PLL registers

     Along with the above values, could you please change this value as well in the same file "clocks_ti816x.h". (I found this error in 675MHz settings, as a safety measure)

    -#define DDR_INTFREQ3           0x13
    +#define DDR_INTFREQ3          13

    Regards

    AnilKumar

    Please mark this Forum post as answered via the Verify Answer button below if it helps answer your question.  Thanks!

  • Hi,AnilKumar

    Thank you for your answer, but  following your answer,  I still had not seen values changed in the DDR_PLL registers.

  • Lingyi Ying,

    Could you provide the bootlog (from power-up) and DDR_PLL registers dump from u-boot?

     TI8168_EVM#md 0x48140440

    Regards

    AnilKumar

    Please mark this Forum post as answered via the Verify Answer button below if it helps answer your question.  Thanks!

  • anli is right,

    you should change both clocks_ti816x.h and ddr_defs_ti816x.h.

    It works on my board.

    I changed it to 400Mhz. It shows like below

                                                                                   
    TI8168-GP rev 1.1

    ARM clk: 987MHz
    DDR clk: 398MHz

    I2C: ready
    DRAM: 1 GiB
    NAND: HW ECC Hamming Code selected
    256 MiB

    Regards,

    Lei

  • Hi, AnilKumar

     the bootlog (from power-up) as flowers:

    U-Boot 2010.06 (Nov 10 2011 - 19:25:12)

    DRAM:  2 GiB
    Using default environment

    MMC:   OMAP SD/MMC: 0
    Hit any key to stop autoboot:  0
    raise: Signal # 8 caught
    reading u-boot.bin

    340640 bytes read
    ## Starting application at 0x80800000 ...


    U-Boot 2010.06 (Feb 26 2012 - 21:37:37)

    TI8168-GP rev 1.1

    ARM clk: 987MHz
    DDR clk: 675MHz

    I2C:   ready
    DRAM:  2 GiB
    NAND:  HW ECC Hamming Code selected
    256 MiB
    :,;;:;:;;;;;;;;r;;:,;;:;:;;;;;;;;:,;;:;:;;;;;;;;:,;;:;:;;;;;;;;:;;;;;;;;:,;;:;:
    ;,;:::;;;;r;;;rssiSiS552X5252525259GX2X9hX9X9XX2325S55252i5:,;;:;:;;;;;;;;:,;;:
    ;:;;;;;;;rrssSsS52S22h52299GGAAMHMM#BBH#B#HMM#HMBA&&XX2255S2S5Si:,;;:;:;;;;;;;;
    ;:;;r;;rsrrriiXS5S329&A&MH#BMB#A&9XXA252GXiSXX39AAMMMBB&G22S5i2SSiiiisi:,;;:;:;
    ;;;;;r;rr2iisiih393HB#B#AA99i22irrrX3X52AGsisss2Xii2299HBMA&X2S5S5iSiisSsi:,;;:
    r:r;rrsrsihXSi2&##MHB&Ahh3AGHGA9G9h&#H##@@@##MAMMXXX9SSS29&&HGGX2i5iisiiisisi:,
    ;;rrrrsSiiiA&ABH&A9GAGhAhBAMHA9HM@@@@@@@@@@@@@@@@@@@HHhAh2S2SX9&Gh22SSiisiiisii
    r:rrssisiS2XM##&h3AGAX&3GG3Ssr5H@M#HM2; ;2X&&&MHMB###GBB#B&XXSSs529XX55iSsisisi
    r;rsrisSi2XHAhX99A3XXG&&XS;:,rH#HGhAS   @@@@3rs2XBM@@A552&&AHA2XiisSS252SSsisSs
    r;issi5S22&&3iSSX292&hXsr;;:;h@&G339&S9@@@@2@MA&9&HB##Xris29ABMAAX2ir;rsSi5iss5
    rrsSi2XhG&9GXh399&X99i;;;;;;r#H&293H9X#@@@@@@@B&9GhAH@XrrsrsiXABHB&HG2rr;rrSiSi
    ;:rsisS599&AA9XG&3A35r;:::;,;BMh&&2iX5A@@@@@@@&392X5GB2;;;r;iSX393A##A&Xi:::rsi
    ;:rss552222X553&XHMhir;;::,:,h#HhGSXhG3#@@@@#AXXS2XAHA;::;;;;ss55XShBA3239r:,;;
    r;ii2S5SSi2i53hirsh2srr::,,,,;MMXX359&Ah3h&Si59SX99A#i:,::::;;sri2,.2r;:SGAr;,:
    ;:;rrrrssiriXGSi::shs;;;,,,:,,rBBA9h5s5h5iS5isi2SAHB5:,,,:::;rrs5&SrisSX5Srrr:,
    ;,r;;;;rsriSSrrrr;;5Xrr;;,:,,.,;9AA2SsisS5323XXXG9&i:.,,::;;r;;;srrrrrr;;:;::::
    :,;r;r;rrissrrr;:;::;s;;;;,:,,..,r293h222hXXAAGGGX;:,,,:,:,::;:;::,:,,,,...,,,,
    ;,;;;;rrrrrrrrirr;,.,,:::::::,,,,.,;SX&ABAB2hhXir:,,.,,.,,:,,,,..,,,..,..,,,..:
    :.:;:;;;:;;;;r;rrs;:.. ,,:::::,:,:,,.::rrsrr;;,,.......,..,....,,,,,,,...,.,,:,
    :.:::,::::::;;r;rrr;:.......,.,.,,:::,,...............,,::.,,,,:,::,,:,:,,,:,;:
    ,.::,:,,,,,;;;;;;;;r;;::,..............................;;;:;::::,:::::::,:,:,,,
    : ,,:,,,,,,,,,,,,,:;rrr;;:;,,,,,,,::,.,.:.,.,;s,:;;;;:;:;;;;;::::,:::,:::,:,:,:
    ,.,,,,,,,...,,.,,....................................:,............:,,,:,:,,,,,

    MMC:   OMAP SD/MMC: 0
    Net:   Detected MACID:90:d7:eb:36:39:a4
    Ethernet PHY: GENERIC @ 0x01
    DaVinci EMAC
    Hit any key to stop autoboot:  0
    TI8168_EVM#
    TI8168_EVM#
    TI8168_EVM#md 0x48140440
    48140440: 003b018c 00000000 00000000 00000102    ..;.............
    48140450: 98d99999 0000011e 98000000 00000104    ................
    48140460: 8e000000 00000104 8e000000 00000104    ................
    48140470: 006e028c 00000000 8b000000 00000105    ..n.............
    48140480: 8a000000 00000102 8a000000 00000102    ................
    48140490: 00000000 00000000 00000000 00000000    ................
    481404a0: 00401988 00000000 00000000 00000000    ..@.............
    481404b0: 8e000000 00000104 89000000 00000105    ................
    481404c0: 89cbc148 00000114 8d800000 00000114    H...............
    481404d0: 00000000 00000000 00000000 00000000    ................
    481404e0: 00000000 00000000 00000000 00000000    ................
    481404f0: 00000000 00000000 00000000 00000000    ................
    48140500: 00000000 00000000 00000000 00000000    ................
    48140510: 00000000 00000000 00000000 00000000    ................
    48140520: 00000000 00000000 00000000 00000000    ................
    48140530: 00000000 00000000 00000000 00000000    ................
    TI8168_EVM#

  • Hi Lingyi Ying,

    U-Boot 2010.06 (Nov 10 2011 - 19:25:12)

    This tells me that code was build on November 10th 2011. (First stage)

    Could you please do only the above modifications, build the u-boot (distclean and re-build) and try once again?

    You should use both imges are from recent build.

    Regards

    AnilKumar

    Please mark this Forum post as answered via the Verify Answer button below if it helps answer your question.  Thanks!