Attached logs are taken from DM365 EVM board with encodedecode application ./encodedecode -y 2 -p -r 720x576.
color space UYVY planar
bootargs: mem=70M console=ttyS0,115200n8 root=/dev/nfs rw noinitrd nfsroot=10.0.0.230:/home/sudhanshu/work/evm/target video=davincifb:vid0=OFF:vid1=OFF:osd0=720x576x16,4050K dm365_imp.oper_mode=0 davinci_capture.device_type=4 davinci_enc_mngr.ch0_mode=pal davinci_enc_mngr.ch0_output=COMPOSITE davinci_enc_mngr.ch0_mode=pal
Attached log which shows CPU consumption going upto 25% for nearly 2 minutes before it went back to 0-1 %. Same is observed with top. Most of this is contributed by the display thread which is just doing DQBUF and QBUF.
Anyone who has noticed this issue and has nay suggestions ?
Regards,
Sudhanshu