Hi,
Could you please clarify the behavior of the SOFTRESET Register in the EMAC module (section 18.3.3.34 in the TRM). The manual says this resets the EMAC module only, however after a bit of debugging in the Linux driver it seems that this reset also resets the MDIO module. The MDIO module's control register is set to the default values after a softreset of the mac module. Can you confirm this?Thank you! Regards, Christian