Dear,
Could someone give me your advise for following?
Device: TMS320VC5507ZHH
Following description in spru586b.pdf, TMS320VC5507/5509 DSP ADC Reference Guide, confused me.
In page 8,
ADC Sample and Hold Period = (1/(ADC Clock)) / (2 x (CONVRATEDIV + 1 + SAMPTIMEDIV))
[must be greater than or equal to 40us]
In page 13,
ADC Sample and Hold Period = (ADC Clock Period) x (2 x (CONVRATEDIV + 1 + SAMPTIMEDIV))
Above 2 fomula are inconsistency.
Because (1/(ADC Clock Freq)) = (ADC Clock Period)
<< My Question >>:
I think "In page 13" is right.
If so, I think the "In page 8" should be described as following.
Am I right?
ADC Sample and Hold Period = (1/(ADC Clock)) x (2 x (CONVRATEDIV + 1 + SAMPTIMEDIV))
[must be greater than or equal to 40us]
Page 8.

Page 13.
Thank you and Best regards,
Okayama