This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

C6416 DSK interfacing external ADC/DAC through 5-6 card

Other Parts Discussed in Thread: DAC8554, ADS1174

Hi,

I am using a C6416 DSK board from Spectrum to develop a real time program. I cannot use the onboard AIC23 codec since I need to work with very low frequencies and its cutoff is 10Hz. I have a 5-6 interface card plugged on the DSK system, with the ADS1174 and the DAC8554 modules that provide the input and output for my signals. The problem is that I haven´t found much information about how to interface the DSK and the ADC/DAC through the 5-6 board.

Any references where I could have a look at?. A piece of code to start with would be very useful as well.

Thanks in advance,

Ivan.