Other Parts Discussed in Thread: DAC8554, ADS1174
Hi,
I am using a C6416 DSK board from Spectrum to develop a real time program. I cannot use the onboard AIC23 codec since I need to work with very low frequencies and its cutoff is 10Hz. I have a 5-6 interface card plugged on the DSK system, with the ADS1174 and the DAC8554 modules that provide the input and output for my signals. The problem is that I haven´t found much information about how to interface the DSK and the ADC/DAC through the 5-6 board.
Any references where I could have a look at?. A piece of code to start with would be very useful as well.
Thanks in advance,
Ivan.