This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

how to make 3G HUAWEI E1731 Modem plug and play in Android 2.3.4 and Android 4.0.3



Dear all

i followed the below path

"http://processors.wiki.ti.com/index.php/TI-Android-ICS-PortingGuide#Android_USB_Configuration"

to configure the  HUAWEI E1731 3G dongle  to Android 2.3.4 and Android 4.0.3 and it worked fine by

/////////////////////////////////////////////////////////////////////////////////////////////////////////////////////////////////////////////////////////////////////////////

                                                          xxx.sh

/////////////////////////////////////////////////////////////////////////////////////////////////////////////////////////////////////////////////////////////////////////////

1) mount -t usbfs usbfs /proc/bus/usb
2) /system/xbin/usb_modeswitch -I -W -c /system/xbin/usb_modeswitch.conf
3) /system/bin/pppd /dev/ttyUSB0 115200 persist defaultroute usepeerdns updetach crtscts noauth debug connect "/system/xbin/chat -v -s -f /system/etc/ppp/airtel.chat"
4) setprop net.dns1 <IP1> 5) setprop net.dns2 <IP2>

////////////////////////////////////////////////////////////////////////////////////////////////////////////////////////////////////////////////////////////////////////////

using this above commands and Kernel configuration i success fully connected to the net. and browsed manully executing the commands.

what i want:

But the problem is using these commands 1-5 above i would like to create a shell script "XXX.sh" in /system/bin/
when i plug-in the Usb3G Modem in the usb hub "XXX.sh" should get executed.
I.e., i want to implement the functionality for Plug and Play.


so that i can use Usb3G Modem without any problem.

Could any one suggest me a solution to make it work in plug and play mode with the shell script "XXX.sh".
so that the XXX.sh script gets called when ever the "Usb3G Modem" is plugged-in.
PLATFORM:

BEAGLEBOARD-XM

Regards
Mahaboob A Aslam