hi paul .....
sorry i didn't reach you these many days.
i have a problem with downloading the files from the internet using terminal.
generally from Linux we can download files using the command "wget <path of file>"
same command i used for download files from the net there is two ways i followed
1---------------->
root@10.0.0.7:/opt/dvsdk# wget http://ftp.gnu.org/gnu/wget/wget-1.6.tar.gz
--12:16:16-- http://ftp.gnu.org/gnu/wget/wget-1.6.tar.gz
=> `wget-1.6.tar.gz.1'
Resolving ftp.gnu.org... failed: Temporary failure in name resolution.
but i am getting failed error because of resolution . i tried with ip address of the wed site
2------------------>
root@10.0.0.7:/opt/dvsdk# wget 140.186.70.20/gnu/wget/wget-1.6.tar.gz
--12:16:31-- http://140.186.70.20/gnu/wget/wget-1.6.tar.gz
=> `wget-1.6.tar.gz.1'
Connecting to 140.186.70.20:80... connected.
HTTP request sent, awaiting response... 200 OK
Length: 670,777 (655K) [application/x-gzip]
100%[====================================>] 670,777 133.63K/s ETA 00:00
12:16:38 (121.21 KB/s) - `wget-1.6.tar.gz.1' saved [670777/670777]
now it is working fine
--------------------------------------------------------------------------------------------------------------------------
please tell me how to work the first case . because remembering the ip address is so hard .
thanks for your support on all my issues