Hello!
I have a problem when I install DSP/BIOS PSP drivers version 1.30.00.05. The Installation says it is correctly done. But I think there is some kind of problem when I am setting up the environment variables (I am not sure if I do it the right way). Anyway when I am starting matlab an error message occur see below. Can someone help me with this problem?
At the moment my environment variables are set to: PSP_EVMC6748_INSTALLDIR C:\Program Files\Texas Instruments\pspdrivers_01_30_00_05
Maybe I should install it in an other folder?
checkEnvSetup('ccs','c6748evm','check')Warning: Undefined function or method 'getPspVersion' for input arguments of type
'ticcsext.autointerface.ticcs'.
> In C:\Program Files\MATLAB\R2010a\toolbox\idelink\extensions\ticcs\envChecker\checkEnvSetup_private.p>genReport at 373
In C:\Program Files\MATLAB\R2010a\toolbox\idelink\extensions\ticcs\envChecker\checkEnvSetup_private.p>checkEnvSetup_private at 61
In checkEnvSetup at 131
4. C674x DSP/BIOS PSP Drivers
Your version :
Required version: 1.30.00.05
Required by : Embedded IDE Link 4.1
Required for : Code generation / device drivers
PSP_EVMC6748_INSTALLDIR="C:\Program Files\Texas Instruments\pspdrivers_01_30_00_05"
>>
checkEnvSetup('ccs','c6748evm','setup')
4. Checking C674x DSP/BIOS PSP Drivers version
Required version: 1.30.00.05
Required by : Embedded IDE Link 4.1
Required for : Code generation / device drivers
Warning: Undefined function or method 'getPspVersion' for input arguments of type
'ticcsext.autointerface.ticcs'.
> In C:\Program Files\MATLAB\R2010a\toolbox\idelink\extensions\ticcs\envChecker\checkEnvSetup_private.p>envSetup at 285
In C:\Program Files\MATLAB\R2010a\toolbox\idelink\extensions\ticcs\envChecker\checkEnvSetup_private.p>checkEnvSetup_private at 68
In checkEnvSetup at 131
Your Version :
Incompatible version detected. C674x DSP/BIOS PSP Drivers version does not satisfy product requirements!
Following environment variables required for code generation could not be set:
### "PSP_EVMC6748_INSTALLDIR"
>>