This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hardware:
MSP430F5529LP
CC3100 Booster Pack on v1.0.0.1 firmware
This TI tutorial is what I have been trying to follow in order to get the CC3100 connected to the internet.
When I attempt to connect to the internet, it seems like the device just hangs at the initial prompt, which you can see in the screenshot below:
Something to note is that I only have access to WPA2-Enterprise and my phone's Wifi signals. I have been using my phone's access point feature with the same SSID and security type as what I have set up in sl_common.h. My laptop can connect to this network and access the internet just fine. However, the CC3100 keeps attempting to obtain an IP address to no avail. Can someone please provide some insight?