This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi we're charging two 50F 2.7V SCAPs in series from a 14V input and were thinking of using two TPS62150 chips one set to 5.4V and the other to 2.7V to keep the caps from hogging voltage. The thing is that these caps draw a large load and the TPS62150 will go into current control. Can they handle being pushed to their limit without adverse affects? Is there a better chip that will handle series charging?
Thank you,
R Dee
Design Specialties