Uptime and system time are jumping ahead.
we made a deeper analysys and we found that jiffies value jumps aswell.
The value of the jump is 131072 secs and it's excacltly like the value of parameter KTIME_MAX.
Is it possible that the timekeeping add this value to jiffies value?
Which could be the condition in order this thing can happen?
The issue is absolutely random so we cannot state when it will succeed.
here's our .config of a Variscite board mounting AM 3517.
The srange thing is that all seems ok (the system believes that the uptime is real) but instead it's 1024 secs less.
These jumps are frequent (1 2 times a day) after a random startup time (averare after 1,5 day).
Any idea?
#
# Automatically generated make config: don't edit
# Linux kernel version: 2.6.32
# Thu Jul 28 15:13:48 2011
#
CONFIG_ARM=y
CONFIG_HAVE_PWM=y
CONFIG_SYS_SUPPORTS_APM_EMULATION=y
CONFIG_GENERIC_GPIO=y
CONFIG_GENERIC_TIME=y
CONFIG_GENERIC_CLOCKEVENTS=y
CONFIG_GENERIC_HARDIRQS=y
CONFIG_STACKTRACE_SUPPORT=y
CONFIG_HAVE_LATENCYTOP_SUPPORT=y
CONFIG_LOCKDEP_SUPPORT=y
CONFIG_TRACE_IRQFLAGS_SUPPORT=y
CONFIG_HARDIRQS_SW_RESEND=y
CONFIG_GENERIC_IRQ_PROBE=y
CONFIG_RWSEM_GENERIC_SPINLOCK=y
CONFIG_ARCH_HAS_CPUFREQ=y
CONFIG_GENERIC_HWEIGHT=y
CONFIG_GENERIC_CALIBRATE_DELAY=y
CONFIG_GENERIC_HARDIRQS_NO__DO_IRQ=y
CONFIG_VECTORS_BASE=0xffff0000
CONFIG_DEFCONFIG_LIST="/lib/modules/$UNAME_RELEASE/.config"
CONFIG_CONSTRUCTORS=y
#
# General setup
#
CONFIG_EXPERIMENTAL=y
CONFIG_BROKEN_ON_SMP=y
CONFIG_INIT_ENV_ARG_LIMIT=32
CONFIG_LOCALVERSION=""
# CONFIG_LOCALVERSION_AUTO is not set
CONFIG_SWAP=y
CONFIG_SYSVIPC=y
CONFIG_SYSVIPC_SYSCTL=y
# CONFIG_POSIX_MQUEUE is not set
CONFIG_BSD_PROCESS_ACCT=y
# CONFIG_BSD_PROCESS_ACCT_V3 is not set
# CONFIG_TASKSTATS is not set
# CONFIG_AUDIT is not set
#
# RCU Subsystem
#
CONFIG_TREE_RCU=y
# CONFIG_TREE_PREEMPT_RCU is not set
# CONFIG_TINY_RCU is not set
# CONFIG_RCU_TRACE is not set
CONFIG_RCU_FANOUT=32
# CONFIG_RCU_FANOUT_EXACT is not set
# CONFIG_TREE_RCU_TRACE is not set
CONFIG_IKCONFIG=y
CONFIG_IKCONFIG_PROC=y
CONFIG_LOG_BUF_SHIFT=14
CONFIG_GROUP_SCHED=y
CONFIG_FAIR_GROUP_SCHED=y
# CONFIG_RT_GROUP_SCHED is not set
CONFIG_USER_SCHED=y
# CONFIG_CGROUP_SCHED is not set
# CONFIG_CGROUPS is not set
CONFIG_SYSFS_DEPRECATED=y
CONFIG_SYSFS_DEPRECATED_V2=y
# CONFIG_RELAY is not set
# CONFIG_NAMESPACES is not set
CONFIG_BLK_DEV_INITRD=y
CONFIG_INITRAMFS_SOURCE=""
CONFIG_RD_GZIP=y
# CONFIG_RD_BZIP2 is not set
# CONFIG_RD_LZMA is not set
CONFIG_CC_OPTIMIZE_FOR_SIZE=y
CONFIG_SYSCTL=y
CONFIG_ANON_INODES=y
CONFIG_EMBEDDED=y
CONFIG_UID16=y
# CONFIG_SYSCTL_SYSCALL is not set
CONFIG_KALLSYMS=y
CONFIG_KALLSYMS_ALL=y
CONFIG_KALLSYMS_EXTRA_PASS=y
CONFIG_HOTPLUG=y
CONFIG_PRINTK=y
CONFIG_BUG=y
CONFIG_ELF_CORE=y
CONFIG_BASE_FULL=y
CONFIG_FUTEX=y
CONFIG_EPOLL=y
CONFIG_SIGNALFD=y
CONFIG_TIMERFD=y
CONFIG_EVENTFD=y
CONFIG_SHMEM=y
CONFIG_AIO=y
#
# Kernel Performance Events And Counters
#
CONFIG_VM_EVENT_COUNTERS=y
CONFIG_COMPAT_BRK=y
CONFIG_SLAB=y
# CONFIG_SLUB is not set
# CONFIG_SLOB is not set
# CONFIG_PROFILING is not set
CONFIG_HAVE_OPROFILE=y
# CONFIG_KPROBES is not set
CONFIG_HAVE_KPROBES=y
CONFIG_HAVE_KRETPROBES=y
CONFIG_HAVE_CLK=y
#
# GCOV-based kernel profiling
#
# CONFIG_GCOV_KERNEL is not set
# CONFIG_SLOW_WORK is not set
CONFIG_HAVE_GENERIC_DMA_COHERENT=y
CONFIG_SLABINFO=y
CONFIG_RT_MUTEXES=y
CONFIG_BASE_SMALL=0
CONFIG_MODULES=y
# CONFIG_MODULE_FORCE_LOAD is not set
CONFIG_MODULE_UNLOAD=y
# CONFIG_MODULE_FORCE_UNLOAD is not set
CONFIG_MODVERSIONS=y
CONFIG_MODULE_SRCVERSION_ALL=y
CONFIG_BLOCK=y
CONFIG_LBDAF=y
# CONFIG_BLK_DEV_BSG is not set
# CONFIG_BLK_DEV_INTEGRITY is not set
#
# IO Schedulers
#
CONFIG_IOSCHED_NOOP=y
CONFIG_IOSCHED_DEADLINE=y
CONFIG_IOSCHED_CFQ=y
# CONFIG_DEFAULT_DEADLINE is not set
CONFIG_DEFAULT_CFQ=y
# CONFIG_DEFAULT_NOOP is not set
CONFIG_DEFAULT_IOSCHED="cfq"
# CONFIG_INLINE_SPIN_TRYLOCK is not set
# CONFIG_INLINE_SPIN_TRYLOCK_BH is not set
# CONFIG_INLINE_SPIN_LOCK is not set
# CONFIG_INLINE_SPIN_LOCK_BH is not set
# CONFIG_INLINE_SPIN_LOCK_IRQ is not set
# CONFIG_INLINE_SPIN_LOCK_IRQSAVE is not set
CONFIG_INLINE_SPIN_UNLOCK=y
# CONFIG_INLINE_SPIN_UNLOCK_BH is not set
CONFIG_INLINE_SPIN_UNLOCK_IRQ=y
# CONFIG_INLINE_SPIN_UNLOCK_IRQRESTORE is not set
# CONFIG_INLINE_READ_TRYLOCK is not set
# CONFIG_INLINE_READ_LOCK is not set
# CONFIG_INLINE_READ_LOCK_BH is not set
# CONFIG_INLINE_READ_LOCK_IRQ is not set
# CONFIG_INLINE_READ_LOCK_IRQSAVE is not set
CONFIG_INLINE_READ_UNLOCK=y
# CONFIG_INLINE_READ_UNLOCK_BH is not set
CONFIG_INLINE_READ_UNLOCK_IRQ=y
# CONFIG_INLINE_READ_UNLOCK_IRQRESTORE is not set
# CONFIG_INLINE_WRITE_TRYLOCK is not set
# CONFIG_INLINE_WRITE_LOCK is not set
# CONFIG_INLINE_WRITE_LOCK_BH is not set
# CONFIG_INLINE_WRITE_LOCK_IRQ is not set
# CONFIG_INLINE_WRITE_LOCK_IRQSAVE is not set
CONFIG_INLINE_WRITE_UNLOCK=y
# CONFIG_INLINE_WRITE_UNLOCK_BH is not set
CONFIG_INLINE_WRITE_UNLOCK_IRQ=y
# CONFIG_INLINE_WRITE_UNLOCK_IRQRESTORE is not set
# CONFIG_MUTEX_SPIN_ON_OWNER is not set
# CONFIG_FREEZER is not set
#
# System Type
#
CONFIG_MMU=y
# CONFIG_ARCH_AAEC2000 is not set
# CONFIG_ARCH_INTEGRATOR is not set
# CONFIG_ARCH_REALVIEW is not set
# CONFIG_ARCH_VERSATILE is not set
# CONFIG_ARCH_AT91 is not set
# CONFIG_ARCH_CLPS711X is not set
# CONFIG_ARCH_GEMINI is not set
# CONFIG_ARCH_EBSA110 is not set
# CONFIG_ARCH_EP93XX is not set
# CONFIG_ARCH_FOOTBRIDGE is not set
# CONFIG_ARCH_MXC is not set
# CONFIG_ARCH_STMP3XXX is not set
# CONFIG_ARCH_NETX is not set
# CONFIG_ARCH_H720X is not set
# CONFIG_ARCH_NOMADIK is not set
# CONFIG_ARCH_IOP13XX is not set
# CONFIG_ARCH_IOP32X is not set
# CONFIG_ARCH_IOP33X is not set
# CONFIG_ARCH_IXP23XX is not set
# CONFIG_ARCH_IXP2000 is not set
# CONFIG_ARCH_IXP4XX is not set
# CONFIG_ARCH_L7200 is not set
# CONFIG_ARCH_DOVE is not set
# CONFIG_ARCH_KIRKWOOD is not set
# CONFIG_ARCH_LOKI is not set
# CONFIG_ARCH_MV78XX0 is not set
# CONFIG_ARCH_ORION5X is not set
# CONFIG_ARCH_MMP is not set
# CONFIG_ARCH_KS8695 is not set
# CONFIG_ARCH_NS9XXX is not set
# CONFIG_ARCH_W90X900 is not set
# CONFIG_ARCH_PNX4008 is not set
# CONFIG_ARCH_PXA is not set
# CONFIG_ARCH_MSM is not set
# CONFIG_ARCH_RPC is not set
# CONFIG_ARCH_SA1100 is not set
# CONFIG_ARCH_S3C2410 is not set
# CONFIG_ARCH_S3C64XX is not set
# CONFIG_ARCH_S5PC1XX is not set
# CONFIG_ARCH_SHARK is not set
# CONFIG_ARCH_LH7A40X is not set
# CONFIG_ARCH_U300 is not set
# CONFIG_ARCH_DAVINCI is not set
CONFIG_ARCH_OMAP=y
# CONFIG_ARCH_BCMRING is not set
# CONFIG_ARCH_U8500 is not set
#
# TI OMAP Implementations
#
CONFIG_ARCH_OMAP_OTG=y
# CONFIG_ARCH_OMAP1 is not set
# CONFIG_ARCH_OMAP2 is not set
CONFIG_ARCH_OMAP3=y
# CONFIG_ARCH_OMAP4 is not set
#
# OMAP Feature Selections
#
CONFIG_OMAP_RESET_CLOCKS=y
CONFIG_OMAP_MUX=y
# CONFIG_OMAP_MUX_DEBUG is not set
CONFIG_OMAP_MUX_WARNINGS=y
CONFIG_OMAP_MCBSP=y
# CONFIG_OMAP_MBOX_FWK is not set
# CONFIG_OMAP_MPU_TIMER is not set
CONFIG_OMAP_32K_TIMER=y
# CONFIG_OMAP3_DEBOBS is not set
CONFIG_OMAP_32K_TIMER_HZ=128
CONFIG_OMAP_DM_TIMER=y
# CONFIG_OMAP_LL_DEBUG_UART1 is not set
# CONFIG_OMAP_LL_DEBUG_UART2 is not set
CONFIG_OMAP_LL_DEBUG_UART3=y
# CONFIG_OMAP_LL_DEBUG_NONE is not set
# CONFIG_OMAP_PM_NONE is not set
CONFIG_OMAP_PM_NOOP=y
# CONFIG_OMAP_PM_SRF is not set
CONFIG_ARCH_OMAP34XX=y
CONFIG_ARCH_OMAP3430=y
CONFIG_OMAP_PACKAGE_CBB=y
#
# OMAP Board Type
#
# CONFIG_MACH_OMAP3_BEAGLE is not set
# CONFIG_MACH_OMAP_LDP is not set
# CONFIG_MACH_OVERO is not set
# CONFIG_MACH_OMAP3EVM is not set
# CONFIG_MACH_VAR_SOM_OM3X is not set
CONFIG_MACH_VAR_SOM_AM35=y
# CONFIG_MACH_OMAP3517EVM is not set
CONFIG_PMIC_TPS65023=y
# CONFIG_MACH_OMAP3_PANDORA is not set
# CONFIG_MACH_OMAP3_TOUCHBOOK is not set
# CONFIG_MACH_OMAP_3430SDP is not set
# CONFIG_MACH_NOKIA_RX51 is not set
# CONFIG_MACH_OMAP_ZOOM2 is not set
# CONFIG_MACH_OMAP_ZOOM3 is not set
# CONFIG_MACH_CM_T35 is not set
# CONFIG_MACH_IGEP0020 is not set
# CONFIG_MACH_OMAP_3630SDP is not set
# CONFIG_OMAP3_EMU is not set
# CONFIG_OMAP3_SDRC_AC_TIMING is not set
#
# Processor Type
#
CONFIG_CPU_32=y
CONFIG_CPU_32v6K=y
CONFIG_CPU_V7=y
CONFIG_CPU_32v7=y
CONFIG_CPU_ABRT_EV7=y
CONFIG_CPU_PABRT_V7=y
CONFIG_CPU_CACHE_V7=y
CONFIG_CPU_CACHE_VIPT=y
CONFIG_CPU_COPY_V6=y
CONFIG_CPU_TLB_V7=y
CONFIG_CPU_HAS_ASID=y
CONFIG_CPU_CP15=y
CONFIG_CPU_CP15_MMU=y
#
# Processor Features
#
CONFIG_ARM_THUMB=y
# CONFIG_ARM_THUMBEE is not set
# CONFIG_CPU_ICACHE_DISABLE is not set
# CONFIG_CPU_DCACHE_DISABLE is not set
# CONFIG_CPU_BPREDICT_DISABLE is not set
CONFIG_HAS_TLS_REG=y
CONFIG_ARM_L1_CACHE_SHIFT=6
CONFIG_ARM_ERRATA_430973=y
CONFIG_ARM_ERRATA_458693=y
CONFIG_ARM_ERRATA_460075=y
CONFIG_COMMON_CLKDEV=y
#
# Bus support
#
# CONFIG_PCI_SYSCALL is not set
# CONFIG_ARCH_SUPPORTS_MSI is not set
# CONFIG_PCCARD is not set
#
# Kernel Features
#
CONFIG_TICK_ONESHOT=y
CONFIG_NO_HZ=y
# CONFIG_HIGH_RES_TIMERS is not set
CONFIG_GENERIC_CLOCKEVENTS_BUILD=y
CONFIG_VMSPLIT_3G=y
# CONFIG_VMSPLIT_2G is not set
# CONFIG_VMSPLIT_1G is not set
CONFIG_PAGE_OFFSET=0xC0000000
CONFIG_PREEMPT_NONE=y
# CONFIG_PREEMPT_VOLUNTARY is not set
# CONFIG_PREEMPT is not set
CONFIG_HZ=128
# CONFIG_THUMB2_KERNEL is not set
CONFIG_AEABI=y
CONFIG_OABI_COMPAT=y
CONFIG_ARCH_HAS_HOLES_MEMORYMODEL=y
# CONFIG_ARCH_SPARSEMEM_DEFAULT is not set
# CONFIG_ARCH_SELECT_MEMORY_MODEL is not set
# CONFIG_HIGHMEM is not set
CONFIG_SELECT_MEMORY_MODEL=y
CONFIG_FLATMEM_MANUAL=y
# CONFIG_DISCONTIGMEM_MANUAL is not set
# CONFIG_SPARSEMEM_MANUAL is not set
CONFIG_FLATMEM=y
CONFIG_FLAT_NODE_MEM_MAP=y
CONFIG_PAGEFLAGS_EXTENDED=y
CONFIG_SPLIT_PTLOCK_CPUS=4
# CONFIG_PHYS_ADDR_T_64BIT is not set
CONFIG_ZONE_DMA_FLAG=0
CONFIG_VIRT_TO_BUS=y
# CONFIG_KSM is not set
CONFIG_DEFAULT_MMAP_MIN_ADDR=4096
# CONFIG_LEDS is not set
CONFIG_ALIGNMENT_TRAP=y
# CONFIG_UACCESS_WITH_MEMCPY is not set
#
# Boot options
#
CONFIG_ZBOOT_ROM_TEXT=0x0
CONFIG_ZBOOT_ROM_BSS=0x0
CONFIG_CMDLINE="root=/dev/nfs nfsroot=192.168.0.1:/home/user/buildroot ip=192.168.0.2:192.168.0.1:192.168.0.1:255.255.255.0:tgt:eth0:off rw console=ttyS2,115200n8"
# CONFIG_XIP_KERNEL is not set
# CONFIG_KEXEC is not set
here we have some configs
12:16:32 up 2 days, 15:23, load average: 0.27, 0.10, 0.05
cpu 1135559 0 149392 21532057 592 266 2856 0 0 0
cpu0 1135559 0 149392 21532057 592 266 2856 0 0 0
intr 6894677 0 0 0 0 0 0 0 0 0 0 0 0 5387 0 0 0 0 0 0 0 0 0 0 0 0 2 0 0 0 0 0 0 0 0 0 0 0 5541750 0 0 0 0 0 0 0 0 0 0 0 0 0 0 0 0 0 0 427968 0 0 0 0 0 0 0 0 0 0 0 789325 123173 0 1 0 1 128 0 0 0 0 0 0 0 0 6942 0 0 0 0 0 0 0 0 0 0 0 0 0 0 0 0 0 0 0 0 0 0 0 0 0 0 0 0 0 0 0 0 0 0 0 0 0 0 0 0 0 0 0 0 0 0 0 0 0 0 0 0 0 0 0 0 0 0 0 0 0 0 0 0 0 0 0 0 0 0 0 0 0 0 0 0 0 0 0 0 0 0 0 0 0 0 0 0 0 0 0 0 0 0 0 0 0 0 0 0 0 0 0 0 0 0 0 0 0 0 0 0 0 0 0 0 0 0 0 0 0 0 0 0 0 0 0 0 0 0 0 0 0 0 0 0 0 0 0 0 0 0 0 0 0 0 0 0 0 0 0 0 0 0 0 0 0 0 0 0 0 0 0 0 0 0 0 0 0 0 0 0 0 0 0 0 0 0 0 0 0 0 0 0 0 0 0 0 0 0 0 0 0 0 0 0 0 0 0 0 0 0 0 0 0 0 0 0 0 0 0 0 0 0 0 0 0 0 0 0 0 0 0 0 0 0 0 0 0 0 0 0 0 0 0 0 0 0 0 0 0 0 0 0 0 0 0 0 0 0 0 0 0 0 0 0 0 0 0 0 0 0 0 0 0 0 0 0 0 0 0 0 0 0 0 0 0 0 0 0 0 0 0 0
ctxt 42825615
btime 1311792785
processes 97158
procs_running 1
procs_blocked 0
softirq 7123779 0 5542277 142608 912533 0 0 130 0 0 526231
228207.09 215320.57
Timer List Version: v0.5
HRTIMER_MAX_CLOCK_BASES: 2
now at 228207106378568 nsecs
cpu: 0
clock 0:
.base: c0494700
.index: 0
.resolution: 7812500 nsecs
.get_time: ktime_get_real
active timers:
clock 1:
.base: c0494728
.index: 1
.resolution: 7812500 nsecs
.get_time: ktime_get
active timers:
#0: <cfaafb70>, hrtimer_wakeup, S:01
# expires at 228207108380766-228207108430766 nsecs [in 2002198 to 2052198 nsecs]
#1: <cfb5de70>, hrtimer_wakeup, S:01
# expires at 228207164819206-228207164869206 nsecs [in 58440638 to 58490638 nsecs]
#2: <cfb87b70>, hrtimer_wakeup, S:01
# expires at 228207328943266-228207329943235 nsecs [in 222564698 to 223564667 nsecs]
#3: <cfa89e70>, hrtimer_wakeup, S:01
# expires at 228207695550206-228207695600206 nsecs [in 589171638 to 589221638 nsecs]
#4: <cf811e70>, hrtimer_wakeup, S:01
# expires at 228207703912206-228207703962206 nsecs [in 597533638 to 597583638 nsecs]
#5: <cfa97e70>, hrtimer_wakeup, S:01
# expires at 228207767175206-228207767225206 nsecs [in 660796638 to 660846638 nsecs]
#6: <cfbc3b70>, hrtimer_wakeup, S:01
# expires at 228207938196195-228207939196164 nsecs [in 831817627 to 832817596 nsecs]
#7: <cd86df38>, hrtimer_wakeup, S:01
# expires at 228208326745999-228208326795999 nsecs [in 1220367431 to 1220417431 nsecs]
#8: <cd807e70>, hrtimer_wakeup, S:01
# expires at 228208484796206-228208484846206 nsecs [in 1378417638 to 1378467638 nsecs]
#9: <cd875e70>, hrtimer_wakeup, S:01
# expires at 228210226922206-228210226972206 nsecs [in 3120543638 to 3120593638 nsecs]
#10: <cfba9e70>, hrtimer_wakeup, S:01
# expires at 228210313043206-228210313093206 nsecs [in 3206664638 to 3206714638 nsecs]
#11: <cfacff38>, hrtimer_wakeup, S:01
# expires at 228212665094389-228212665144389 nsecs [in 5558715821 to 5558765821 nsecs]
#12: <cd871e70>, hrtimer_wakeup, S:01
# expires at 228212825030206-228212825080206 nsecs [in 5718651638 to 5718701638 nsecs]
#13: <cd805e70>, hrtimer_wakeup, S:01
# expires at 228213173913206-228213173963206 nsecs [in 6067534638 to 6067584638 nsecs]
#14: <cfb8de70>, hrtimer_wakeup, S:01
# expires at 228216047326724-228216047376724 nsecs [in 8940948156 to 8940998156 nsecs]
#15: <cfbabe70>, hrtimer_wakeup, S:01
# expires at 228222123695206-228222123745206 nsecs [in 15017316638 to 15017366638 nsecs]
#16: <cd879b70>, hrtimer_wakeup, S:01
# expires at 228224453607571-228224473607571 nsecs [in 17347229003 to 17367229003 nsecs]
#17: <cd877e70>, hrtimer_wakeup, S:01
# expires at 228235842303206-228235842353206 nsecs [in 28735924638 to 28735974638 nsecs]
#18: <cfaa1ad8>, hrtimer_wakeup, S:01
# expires at 228324555383695-228324655383695 nsecs [in 117449005127 to 117549005127 nsecs]
#19: <cfabbad8>, hrtimer_wakeup, S:01
# expires at 228507079004301-228507179004301 nsecs [in 299972625733 to 300072625733 nsecs]
#20: <cfb43e70>, hrtimer_wakeup, S:01
# expires at 228604761101724-228604761151724 nsecs [in 397654723156 to 397654773156 nsecs]
#21: <cd855e70>, hrtimer_wakeup, S:01
# expires at 230318244264206-230318244314206 nsecs [in 2111137885638 to 2111137935638 nsecs]
.nohz_mode : 1
.idle_tick : 228206890625000 nsecs
.tick_stopped : 0
.idle_jiffies : 29172082
.idle_calls : 4812405
.idle_sleeps : 1965533
.idle_entrytime : 228207070154202 nsecs
.idle_waketime : 228206914148355 nsecs
.idle_exittime : 228206914239908 nsecs
.idle_sleeptime : 212510871980193 nsecs
.last_jiffies : 29172104
.next_jiffies : 29172105
.idle_expires : 228206914062500 nsecs
jiffies: 29172109
Tick Device: mode: 1
Per CPU device: 0
Clock Event Device: gp timer
max_delta_ns: 2147483647
min_delta_ns: 91553
mult: 140737
shift: 32
mode: 3
next_event: 228207109375000 nsecs
set_next_event: omap2_gp_timer_set_next_event
set_mode: omap2_gp_timer_set_mode
event_handler: tick_nohz_handler
cat /proc/uptime : 228207.11 215320.57