This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi Team,
Can you help recommend several ICs for LED? Thanks.
Requirements are as follows:
1. 1.5V/1A and 18V/1A
2. Keep it as simple as possible, similar to the image below.
3. Keep the price as low as possible.
Regards, Charlie
Hi Charlie,
what do you mean of "1.5V/1A and 18V/1A"? Is it the input voltage?
BR
Patrick
Hi Patrick,
In practical applications, 5V input or 18V input, and the Iout is no more than 1A. 5V input is preferred as it is cheaper. Thanks.
Regards, Charlie
Hi Charlie,
Could you give a more specific LED current requirement? I think "no more than 1A" is too general.
And how many LEDs in a series?
BR
Patrick