Hi, everyone,
TPS65982 doesn't support PPS (PD 3.0).
Is my understainding right?
When we attach Goppa ATREG27W_03 to our prducts using TPS56982,
TPS65982 requests PPS (3.3V-11V Max. 3A), and repeats hard reset.
On the other hands, when we attach Aukey PA-Y10,
TPS65982 requests fixed PDO (20V Max. 2.3A) correctly,
except PPS (3V-16V Max. 3A).
Best Regards,