This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Good morning TI,
In our proyect we have to transmit one photo of the sensor OV2640 2Mpx (I've attached the detailed PIN) to 1.5 meters. Here is the problem , we can't transmit the signal directly, so I think I need a LVDS right?
I've never used before. Will I get the same signal? Which do you recomend me?
Any information would be highly appreciated.
Thank you
Pin nº | Name | Pin nº | Name | Pin nº | Name |
---|---|---|---|---|---|
1 | NC | 9 | HSYNC | 17 | PCLK |
2 | AGND | 10 | DVDD | 18 | DATA6 |
3 | SDA | 11 | DOVDD | 19 | DATA2 |
4 | AVDD | 12 | DATA9 | 20 | DATA5 |
5 | SCL | 13 | MCLK | 21 | DATA3 |
6 | RESET | 14 | DATA8 | 22 | DATA4 |
7 | VSYNC | 15 | AGND | 23 | DATA1 |
8 | PWDN | 16 | DATA7 | 24 | DATA0 |
I've founded DS90C241/DS90C124 and DS90UR241Q/124Q. What is the difference between them? Will it works with the camera OV2640?
Thank you
Hi Guillermo,
The main difference between the C and the UR parts is the UR parts will randomize the data that's sent over the serial link. This is helpful for emissions. Another difference is the maximum pixel clock rate, which is 35 MHz on the C parts and 43 MHz on the UR parts.
What is your pixel clock rate? The parts you mentioned should work with that Omnivision sensor provided the pixel clock is within the recommended range. You would just ground the unused input pins.
You could also look at the DS90UB913/914 if you wanted an I2C backchannel to communicate over.
Thanks!
Jason Blackman
Hi Jason,
I decided to use DS90UR241/124 because the sensor OV2640 use 36Mhz pixel clock.
I've copied the desgin of the Evaluation board(www.ti.com/tool/serdesur-43usb) and they don't work.
I've attached my design and what I've done.
1.- I've checked the intensity with 3.3V and is 10mA each.
2.- I've verifed input clock and input data signals meet requirements for VILmin, VILmax,
VIHmin, VIHmax, tset, thold.
3.-I've ground the unused pins in the serializer.
Do you know what can it be? What should i have to do?
Thanks, I hope your answer
Hi,
right now, I'm trying start up the camera OV2640, but the camera doesn't work.
I don't know if it's a power problem, if the camera is damage or if I'm missing something in the initialization of the camera.
Voltage power suppy:
AVDD =3V
DVDD=1.3V
DOVDD=3V
AVDD and D0VDD are separated by R/C filter, as shown in "OV2640 Camera Module Hardware Application Notes".
SCCB bus =1,8V
XCLK=24MHz external oscillator.
Initialization on OV2640:
XCLK=active
PWDR=low
RESET=high
SCCB_CLK=high
SCCB_DATA=high
After initialization, PCLK should be running, and HREF,VSYNC AND d[9:0] generate output, but that didn't happen.
I also tried to read and write registers of the camera and it has been impossible.
Could someone tell me if I'm doing something wrong or if the camera is damage.
The test I have done with several cameras.
Thanks,
Diana.