Hi,
ESD protection measures coming from SPI-I / F
The device of SPI interface is corrupted by ESD.
* Since the SPI interfaces with the external device, it is connected to the connector.
Please tell me the best solution for ESD protection measures.
I am considering the following two methods.
1. Use digital isolation to protect the device from ESD from the SPI.
※ Please introduce the device of digital isolator suitable for SPI.
2. Connect the protection diode of ESD (TVS) to the signal line.
※ Please introduce ESD device suitable for SPI.
best regards
cafain