Other Parts Discussed in Thread: TPS25200, LP3878-ADJ
1) I need a 5V, 0.5A , 4kV isolated DC-DC from my 5V power to drive USB 2.0 VBUS pin.
This is for medical application, hence 4KV is needed but the board space is limtied.
Can I use a smaller LDO at the output of transformer instead of TPS76728-EP from the SN6505 eval board?
I assume 4kV is tested between the Ground so LDO at the output should be OK.
2) Since we need a current limit of 0.5A, I'm using PTC and TPS25200.
Would it be better to put TPS25200 on the system side (isolated), instead of the line side.
OR we can use LDO with output current limit.