This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

  • Resolved

ISO1540: Can I parallel ISO1540?

Genius 3885 points

Replies: 4

Views: 516

Part Number: ISO1540

Can I parallel multiple ISO1540s to use one I2C bus to talk to multiple isolated I2C slaves with different address? I assume so, but would like to confirm it before placing it in my design

Thanks!

  • Hi David,

    Thanks for asking your question on E2E and for providing a quick sketch. 

    In short, yes this is fine. For more details please see this E2E thread. 

    Please let me know if you have any additional questions!

    Best regards, 

    Dan

  • In reply to Dan Kisling:

    Thanks, and I followed your link to see the other thread, the diagram in the other thread seems to have the wrong usage on the isolator? I think the single master should be the one sends out the clock to multiple slaves, so the direction of SCL is wrong. If ISO1541 is indeed used like the schematic, side 1 should be the input side, side 2 should be the output side, meaning side 1 should be in the bus side, while side 2 in the device side.

    Could you take another look at that and clarify it?
  • In reply to David Chance:

    Hi David,
    Thanks for catching that. Yes, the direction of SCL does look incorrect. Let me check this with our resident I2C expert on Monday to make sure that I provide you with the best information. Sorry for the inconvenience.
    Best regards,
    Dan
  • In reply to Dan Kisling:

    Hi David,
    Again thanks for pointing out the mistake in our previous post. I've checked in with our resident isolated I2C expert and they confirmed that the drawing was incorrect in the previous post. Please see the following notes.

    1. Side1 always needs to connect to MCU (master/slave) and Side2 to bus.
    2. Slave SCL should be input only, hence ISO1541 can’t be used for slave.
    3. For Slave SCL to work, only ISO1540 should be used.
    4. Only Master can use ISO1541. If it requires clock stretching then it should use ISO1540 only.

    Please let me know if this clarifies the requirement better.
    Thanks and best regards,
    Dan

This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.