Hi Koteshwar,
I am referring the SLLA368B application note for ISOW7840 for Low Emission design. On Page 7 of document it mentions 0.66 mm creepage distance between two Isolated GND ( GND1 and GND2) .
1) Can you tell me this 0.66 mm clearance is ok for 5 KV RMS isolation requirement. On top layer i am considering 1KV / mm . So 5mm for 5KV rms requirement.
2) If there is a Via ( which is from 1st layer to 4th layer) then what should be distance maintained between a track and Via for isolated GND in layer 2 ( Inside layer) I am using FR4 material PCB.
3) can you provide any formula for calculation for Isolation inside layers and if there is a Via.
Regards
harish