This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

  • TI Thinks Resolved

RF Immunity

Prodigy 70 points

Replies: 1

Views: 252

Hi,

We are designing a custom board. We need to meet IEC/EN 61000-4-3 (RF Immunity).

Can anyone share special criteria required for component selection and suggestions to consider while designing? 

  • Hello Sraman,

    There are many resources on TI's web that can assist you.
    One of these is TI Training.

    https://training.ti.com/search-catalog?keywords=IEC%2FEN+61000-4-3&start%5Bdate%5D=&end%5Bdate%5D=

    This will show training topics related to the  IEC specification.

    EMI immunity is platform specific, components, layout.
    You may find information in device product folders.|
    Here is an example.

    TLE2141 and TLE2141-Q1 EMI Immunity Performance
    http://www.ti.com/lit/an/sboz026b/sboz026b.pdf

    "EMI Rejection Ratio (EMIRR)

    The electromagnetic interference (EMI) rejection ratio, or EMIRR, describes the EMI immunity of
    operational amplifiers (op amps). An adverse effect that is common to many op amps is a change in the
    offset voltage as a result of RF signal rectification. An op amp that is more efficient at rejecting this change
    in offset as a result of EMI has a higher EMIRR and is quantified by a decibel value."

    So there are many ways to find information in the TI web.
    If you have device specific questions, create a thread and ENTER A PART NUMBER, in order for the thread to be routed properly.


    Best Regards,

    Ed Walker

This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.