HYi.
void(Init)
{
SSIConfigSetExpClk(SSI1_BASE, SysCtlClockGet(), SSI_FRF_MOTO_MODE_0,SSI_MODE_MASTER, 4000000,8); SSIEnable(SSI1_BASE); GPIOPinTypeSSI(GPIO_PORTE_BASE,GPIO_PIN_0 | GPIO_PIN_3 | GPIO_PIN_2 | GPIO_PIN_1);
}
unsigned char Read_cc2420_RAM(unsigned short adr){ unsigned long l; SSIDataPut(SSI1_BASE,0x80 | (adr & 0x7f)); SSIDataPut(SSI1_BASE,((adr >> 1) & 0xc0) | 0x20); SSIDataGet(SSI1_BASE,&l); return (unsigned char) l;}
void Write_cc2420_RAM(unsigned short adr,unsigned char dat){ SSIDataPut(SSI1_BASE,0x80 | (adr & 0x7f)); SSIDataPut(SSI1_BASE,(adr >> 1) & 0xc0); SSIDataPut(SSI1_BASE,dat); }
int main(void)
RSTnL; RSTnL; RSTnL; RSTnH; VREGenH;
TurnOnOsc();
while(1) {
Write_cc2420_RAM(0x30,0x13); a = Read_cc2420_RAM(0x30); sprintf(pucBuf,"Ram is %3d ",a); RIT128x96x4StringDraw(&pucBuf[0],1, 20, 15);
I get the value of 64 all the time, It looks like the cc2420 returns all the time the status only.
Please Advise
Ephraim Oved
CS.
SI.
SO.