This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Dear Champs,
As it is expected there are so many data throughput will be required on the CAN bus, they would like to separate devices into 2 CAN buses and will send/receive data in each CAN buses simultaneously. For example, 6 devices will be connected to Node1 through CAN bus1 and other 5 devices will be connected to Node 2 through CAN bus2 in below.
Is this possible in AM4372?
Is there any limitation in using 2 x CAN ports simultaneously?
Can each CAN bus reach to 1Mbps speed?
SW is TI-RTOS Processor SDK v6.3.
Thanks and Best Regards,
SI.
SI
I am not aware of any limitations on simultaneously operating both CAN peripherals at full speed.
--Paul