The SensorTag is now released. This is a $25 development kit and reference design for Bluetooth low energy sensor applications. This is the first Bluetooth low energy development kit focusing on wireless sensor applications and it is the only development kit targeting smartphone app developers.
- NO embedded software design knowledge required
- NO embedded compiler required
- iOS sample apps are included to demonstrate use of the sensors(Android sample apps are coming when Android releases an Bluetooth 4.0 API)
The SensorTag includes the following sensors
- Contactless IR temperature sensor (Texas Instruments TMP006)
- Humidity Sensor (Sensirion SHT21)
- Gyroscope (Invensense IMU-3000)
- Accelerometer (Kionix KTXJ9)
- Magnetometer (Freescale MAG3110)
- Barometric pressure sensor (Epcos T5400)
For more information, please see:
SensorTag Wiki:
SensorTag videos:
SensorTag intro and how to use one of TIs most popular tool
Order the SensorTag here.
Best Regards