Now I want to use both uart and spi,uart on port0 and spi on port1,I can not found _hal_uart_spi.c or _hal_uart_isr.c in the project source code in the sample code, but it worked as expected, so the question is where does it be included into the project, and if I want to use both uart and spi, should I add the _hal_uart_spi.c and _hal_uart_isr.c or _hal_uart_dma.c into my project?
Thanks!
Chris