Hi,
I would like to use CC2541's IEEE primary address as an unique identifier of my product. I have three questions regarding that:
(1) Is every CC2541's IEEE primary address guaranteed to be unique?
(2) Is it possible to modify a CC2541's IEEE primary address? I know that the primary address is stored in flash at the location "0x780E-0x7813", so I am wondering if it is possible to use flash programmer to modify it?
(3) How can I force CC2541 to always use IEEE primary address? I know that if the IEEE secondary address is written to anything not FF FF FF FF FF FF, then CC2541 will use secondary address instead of primary address. How can I prevent that?
Regards,
Jack