hi,
I have two modules TiWi-SL EM Board from Ti’s, I am going to use these for sensor applications, so for that I need two host controller. The host controllers that I have chosen are cortexM3 “LPC1769” and ARM7 “LPC2148”. Now my layout is
SENSORS->CortexM3->TiWi-SL (Wirelessly connected) TiWi-SL->ARM7->control measure
Here is my question
1) Are these connections are applicable for WiFi module (ie., TiWi-SL).
2) If it so what are the basic requirements that I have been needed for host control.
3) How can I install the drivers and how I patch these drivers with IAR Embedded workbench for ARM6.30
4) From the host driver which entity that I have been chosen for my application(ie., NVMEM or Socket API or Net App API)
Please guide for me this,
Thanks
best regards,
NIJUS