Hi guys,
I am using the CC3000 and am having problems with the mDNS advertisement . If I set a breakpoint the first time it comes to the function call and from then onwards simply run the program the CC3000 seems to be advertising correctly. However if I simply run the program without setting any breakpoints it looks like the advertisement daemon keeps setting the source address constantly to 0. I have attached the wireshark capture. I have checked ofr delay issues but there doesnt seem to be any. Is this is a bug in the cc3000 firmware?8037.packet_capture.zip