Welcome to the Low Power RF & Wireless Connectivity Section of the TI E2E Support Community. Ask questions, share knowledge, explore ideas, and help solve problems with fellow engineers. To post a question, click on the forum tab then "New Post".
Q: FAQ: How to setup a wireless UART with CC111x/CC251x devices by 1184125
The CC111x/CC251x devices can easily be used to make a standard serial interface like UART wireless. Also covering CRC check and automatic retransmission for error free operation the wireless UART can run with an effective data rate of up to 80 kbps.
Go to http://www.ti.com/litv/zip/swrc088 to download the software.
Documentation can be found on http://www.ti.com/litv/pdf/swru082.
Links are not working.