• Resolved

2812 timer interrupt urgent !

Hello

I was trying to write an assembly program to run an ISR during a timer period interrupt. I had configured all my timer control registers and peripheral clocks required for this. I had also populated the PIE vector table with ".sect directive".  When an interrupt occurs, I can see the interrupt vector ID in the PIECTRL register but the service routine is not getting executed. I suspect it is not at all entering into the ISR. I had been trying this for so long. Kindly help me in this regard.

Regards

Sashank Mani

  • Shashank,

    Are you sure you have all of the interrupts enabled?  Keep in mind that both the global interrupt flag, the global IER register, and the PIE IER register must be setup for an interrupt to execute.

    Trey

    Trey German

    LaunchPad Applications Manager

    If a post answers your question, please mark it with the "verify answer" button.
    Visit these helpful C2000 Links!
    C2000 TI Wiki Pages
    TI Forum Sitemap
    ControlSUITE
    C2000 Getting Started
    CLA FAQs
    Workshop Material!
  • In reply to Trey German289:

    Yes I had initially disabled all the interrupts. I made IER = 0x0000 and disabled PIECTRL. then initialized all sys control registers. initialized timers and then enabled PIEIER. I had followed the flowchart as given in the interrupts reference guide. I was just trying to increment the contents of auxilary register during a period interrupt. Coukd you please give me a sample assembly language program so that I'll get some idea?

  • In reply to shashank mani:

    Shashank,

    While the F2812 isn't really supported within controlSUITE there is still some example software laying around.  I'm not sure if this package will have exactly the assembly code you are looking for, it should have some C examples of how to setup the interrupts.  Take a look at sprc097:

    http://www.ti.com/litv/zip/sprc097

    Trey

    Trey German

    LaunchPad Applications Manager

    If a post answers your question, please mark it with the "verify answer" button.
    Visit these helpful C2000 Links!
    C2000 TI Wiki Pages
    TI Forum Sitemap
    ControlSUITE
    C2000 Getting Started
    CLA FAQs
    Workshop Material!
  • In reply to Trey German289:

    Shashank,

    try defining the ISR function in assmebly as     .sect ".Isr", when we write ISRs in C we have to use interrupt key word, I would assume you will have to do that for assembly routines as well.

    Let us know if it works.

     

    Best Regards

    Santosh

  • In reply to Trey German289:

    I had already seen the mixed source of many c languages to get an idea but unfortunately I couldnt make out anything. Could you please tell me the procedure that has to be followed to service an interrupt in an assembly language? I had initialized the PIE vector table with . sect  and .long directives. Do we need to  follow a sequence while writing these directives. If yes, how does the interrupt source identify that it has to go to a particular offset in the table?

  • In reply to Santosh Athuru:

    I had defined the reset vector with .sect ".reset"  vectors with .sect ".vectors" and Pie vectors with .sect ".pievect". And then using .long directive I had initialized all the interrupt. All the interrupts except the one I am using are made dummy. and then I wrote a MAIN loop. At the end of the main loop, I had USED B MAIN instruction

  • In reply to shashank mani:

    Shashank,

    along with enabling all the interrupt enabled bits (at PIE level, at CPU level (IER) and the EINT) as Trey suggested, you will have to register the handler with PIE (look at examples Trey pointed out at) . As I said along with all above we define ISRs in C with an interrupt key word, so that the assembler can put the right instructions for stack save and return.

    I would suggest to look at the generated assembly for a C-style declared/defines ISR and follow the same in your assembly interrupt routine defnition.

     

    Best Regards

    santosh

  • In reply to Santosh Athuru:

    In the mixed assembly source, He was changing the stackpointer at every interrupt. I thought initializing a PIE vector table and defining an ISR would be an easier task than to manually handle the interrupts

  • In reply to shashank mani:

    This is how I had initialized the table. Kindly tell me what should be the instructions after this if I want to execute Timer1 Period Interrupt.

    VECT:   .sect "vectors"
    .long INIT
    .long ISR1
    .long ISR2
    .long ISR3
    .long ISR4
    .long ISR5
    .long ISR6
    .long ISR7
    .long ISR8
    .long ISR9
    .long ISR10
    .long ISR11
    .long ISR12
    .long ISR13
    .long ISR14

    .sect "pievt"
    PIEVT:
    .long ISR1_1
    .long ISR1_2
    .long ISR1_3
    .long ISR1_4
    .long ISR1_5
    .long ISR1_6
    .long ISR1_7
    .long ISR1_8
    .long ISR2_1
    .long ISR2_2
    .long ISR2_3
    .long SINE
    .long ISR2_5
    .long ISR2_6
    .long ISR2_7
    .long ISR2_8
    .long ISR3_1
    .long ISR3_2
    .long ISR3_3
    .long ISR3_4
    .long ISR3_5
    .long ISR3_6
    .long ISR3_7
    .long ISR3_8
    .long ISR4_1
    .long ISR4_2
    .long ISR4_3
    .long ISR4_4
    .long ISR4_5
    .long ISR4_6
    .long ISR4_7
    .long ISR4_8
    .long ISR5_1
    .long ISR5_2
    .long ISR5_3
    .long ISR5_4
    .long ISR5_5
    .long ISR5_6
    .long ISR5_7
    .long ISR5_8
    .long ISR6_1
    .long ISR6_2
    .long ISR6_3
    .long ISR6_4
    .long ISR6_5
    .long ISR6_6
    .long ISR6_7
    .long ISR6_8
    .long ISR7_1
    .long ISR7_2
    .long ISR7_3
    .long ISR7_4
    .long ISR7_5
    .long ISR7_6
    .long ISR7_7
    .long ISR7_8
    .long ISR8_1
    .long ISR8_2
    .long ISR8_3
    .long ISR8_4
    .long ISR8_5
    .long ISR8_6
    .long ISR8_7
    .long ISR8_8
    .long ISR9_1
    .long ISR9_2
    .long ISR9_3
    .long ISR9_4
    .long ISR9_5
    .long ISR9_6
    .long ISR9_7
    .long ISR9_8
    .long ISR10_1
    .long ISR10_2
    .long ISR10_3
    .long ISR10_4
    .long ISR10_5
    .long ISR10_6
    .long ISR10_7
    .long ISR10_8
    .long ISR11_1
    .long ISR11_2
    .long ISR11_3
    .long ISR11_4
    .long ISR11_5
    .long ISR11_6
    .long ISR11_7
    .long ISR11_8
    .long ISR12_1
    .long ISR12_2
    .long ISR12_3
    .long ISR12_4
    .long ISR12_5
    .long ISR12_6
    .long ISR12_7
    .long ISR12_8

    ; Pie control register. Required to enable PIE
    PIECTRL .set 0x00000CE0

    ; Pie acknowledge register
    PIEACK .set 0x00000CE1

    ; Pie Interrupt Enable Registers
    PIEIER1 .set 0x00000CE2
    PIEIER2 .set 0x00000CE4
    PIEIER3 .set 0x00000CE6
    PIEIER4 .set 0x00000CE8
    PIEIER5 .set 0x00000CEA
    PIEIER6 .set 0x00000CEC
    PIEIER7 .set 0x00000CEE
    PIEIER8 .set 0x00000CF0
    PIEIER9 .set 0x00000CF2
    PIEIER10 .set 0x00000CF4
    PIEIER11 .set 0x00000CF6
    PIEIER12 .set 0x00000CF8

    ; Pie Interrupt flag registers
    PIEIFR1 .set 0x00000CE3
    PIEIFR2 .set 0x00000CE5
    PIEIFR3 .set 0x00000CE7
    PIEIFR4 .set 0x00000CE9
    PIEIFR5 .set 0x00000CEB
    PIEIFR6 .set 0x00000CED
    PIEIFR7 .set 0x00000CEF
    PIEIFR8 .set 0x00000CF1
    PIEIFR9 .set 0x00000CF3
    PIEIFR10 .set 0x00000CF5
    PIEIFR11 .set 0x00000CF7
    PIEIFR12 .set 0x00000CF9
    INIT:
    SETC AMODE
    CLRC OBJMODE
    AND IER, #0x0000
    AND IFR, #0x0000
    //* device peripheral initialization*//
    //*timer initialization*//
  • In reply to shashank mani:

    Shashank,

    where are you placing 'sect  "pievt"' in your memory?

    Best Regards

    santosh