Hello everybody,
I am using a ezdsp TMS320F28335 and after many tests, a new problem is driving me crazy. I am working over a prototipe of full mosfet bridge for stepper motor controlling. And since a couple of days, the board disconnect from the computer while I am working with it (it continue with the program, and it works properly). The message in CCS is this one:
Error: Error 0xA00020A0/-1250 Error during: Execution, Target Communication, Control, Device driver: Lost USB connection to emulator. You should ABORT and restart to re-establish the USB link.
Failed to remove the debug state from the target before disconnecting. There may still be breakpoint opcodes embedded in program memory. It is recommended that you reset the emulator before you connect and reload your program before you continue debugging.
Of course after this I have to remove the power from the board and completely cloes CCS to connect the board again.
Any idea of what can produce this problem?
Thank you in advance.
Ricardo.