Hello,
I have a problem with the adding operation on C28 core (F28M35x). I use the code generation tool and when I would like to add two 32-bit fixed point variables the compiler generates this asm code:
RPT #31
|| SUBCUL ACC,XAR6
MOVL ACC,P
ADDL ACC,XAR7
MOVL *-SP[2],ACC
It takes a lot of time to perform it. Is there any faster way to add two 32-bit values?
Thanks in advance,
Tamas