Hello All
Because our product does not have RS232 interface, there is only a RS485 interface which support Modbus RTU/ASCII.
So We need to develop RS 485 bootloader firmware in TI DSP 28035 as well as PC UI which commmunicate with DSP via RS-485 (ISO 03082) .
Could you please help provide us the method or example on bootLoader via RS-485 (ISO 03082) with TI DSP 28035?
Info:
The CodeSkin primary bootloaders also support communication protocols other than RS-232. For example half-duplex RS-485 and CAN bus. Along with the primary bootloader, the source code of a matching secondary bootloader is provided.