I have the 28035 solar explorer kit. I cannot get the Crosshairs Gui to connect to the board. I get an error window with the following message "Connection could not be established (Connect target failed)" after the Gui screen comes up. I ran the solar workshop labs and have confirmed the JTAG interface works and the board is functional. I reloaded the ControlSuite PVInverter_F2803x.out file into the board to take it back to a known state. I have followed the instructions from the 1067.SolarExplorer_HWGuide.pdf for setting up the connections and receive the error screen when I try to run the Gui:
5.3 GUI Connection
The FTDI chip present on the board can be used as an isolated SCI for communicating with a
HOST i.e. PC. The following jumper settings must be done to enable this connection.
As the GUI software with SCI is provided for F28035 control card only, F28035 settings are
discussed below,
1. Populate the jumper [M7]-J4
2. Remove the jumper [Main]-J4, this disables JTAG connection.
3. For F28035, put SW3 on the F28035 Control Card to OFF position
4. Connect a USB cable from [M7]-JP1 to host PC.
. When I look at the "show" screen for the Gui on the task bar, the listing ends with "2014-Jan-24 13:14:41 - Failed to connect to target with transport: TransportCommros Using method: COMMROS_SERIAL". I'm running a Windows 7 machine with a CCS5 Version: 5.5.0.00077 (not running when I try to use the Gui). I have tried with a second PC running the same software suite and got the same results.
My ultimate use is for the development of an improved MPPT algorithm and want to use the light sensor on board as the peak power point control for testing the algorithms response with the Gui reporting what the maximum power point is. I'm assuming the light sensor is functional in the Gui controller program. My fallback position is to run the kit under CCS, manually set the LightSensor value, and record the maximum panel output and achieved panel output values from the variables in the watch window.
Getting the Gui working would be a lot simpler and be a better looking demonstration for my customer. Any suggestions on how to get the GUI connected?