I am using CCSv4 & CCSv5.4 to write and download programs to controlStick F28069. All of a sudden, I could not download, erase or reprogram my controller. I have then tested and tried using Uniflash programming utility. No success. I have tried reprogramming the FTDI chip with tools addressed in XDS100 page. It seems to be working as expected. I have tried programming another controlStick to make sure that the PC USB is intact. There is no prblem with PC, Software integrity and USB port. I assume FTDI is also clean.
I have tried to see whether any locking and passwords problem. No, I can unlock without error, no unexpected password list. I can read from the memory, but cannot write and cannot program.
I have read many similar discussions, but could not figure out a solution. Before buying a new stick I wanted to get expert opinion. Especially, I am uneasy to get a new device, without knowing the reason of damage or way to cure, if any.
Regards,
Adnan Kurt
PS. This is a typical error message I am getting under Uniflash:
C28xx: Flash Programmer: Error erasing flash memory. << When trying to erase asector
And these are what I get when trying to download a program:
[05:34:01] Loading program: \\PISI\Users\Adnan\ShareVirtual\BlinkingLED.out
[05:34:04] ERROR >> C28xx: Flash Programmer: Error encountered when writing to flash memory
[05:34:05] ERROR >> C28xx: GEL: File: \\PISI\Users\Adnan\ShareVirtual\BlinkingLED.out: Load failed.
[05:34:05] File: \\PISI\Users\Adnan\ShareVirtual\BlinkingLED.out: Load failed.
[05:34:05] Programs operation finished.