I've trying to configure the ADCs in continuous mode, but I need to someone to clarify me some questions,
1. Why in the most examples I found, continuous mode of ADC interruptions, must be disabled in order to obtain max speed? I mean, I don´t understand why, if the intention is that the interrupt triggers the SOCx at the end, what is the proper way then?
2.When accesing to result registry of ADCs structs, this data is allocated on C28 memory, or is accessed trough ACIB, and they are allocated at the Analog Subsystem? Because when i'm try to copy the results to another variable, it takes so long, so I suppose are allocated in Analog Subsystem.
My needs are: the ADCs must performs the conversion continuously as fast as possible, and when my program need, acces to the result registry reading the last conversion performed, it's preferable to no interrupt de processor, I´ve considered the use of the DMA.
Thanks in advance.