Hi, I've just received my F28M35x ISO Control Card (Rev1.0) and I've been failing at loading an example design (ADC soc) from C2000 ControlSuite to the MCUs FLASH. I use CCS 6.0 (with TI 6.2.6 compiler) for the example. Here are what the console said:
Cortex_M3_0: GEL Output: Memory Map Initialization Complete
C28xx_0: GEL Output:
Memory Map Initialization Complete
C28xx_0: GEL Output:
RAM Initialization Complete
C28xx_0: Loader: One or more sections of your program falls into a memory region that is not writable. These regions will not actually be written to the target. Check your linker configuration and/or memory map.
C28xx_0: File Loader: Data verification failed at address 0x0013EB1E Please verify target memory and memory map.
What's going on? I'm sure that my ControlCard is properly powered (led 1 and led 4 are lit). I get power from the docking station. In addition, I also checked JTAG connectivity and everything is fine. I don't think the example is too big to fit the device.