Hi there,
I am currently using the Delfino F28377D on CCS Beta 4 (ver 6.0.0.00156), and I am currently having trouble with the profile clock, as it is not incrementing at all during a debug session. It's remaining on zero the whole time instead.
The program is stepping through the code and updating variables, just not the clock cycles.
In Clock Setup, the Count is on Cycles and the Reset Option on Manual.
Is it a known error, or is there something that I haven't configured properly?
Best Regards,
Corentin