I am wanting to put together a PMSM sensorless controller running with at a loop rate of >50 kHz. I am currently using the f28035 running at 10 kHz, and the ISR uses ~28% of my loop time. I was looking for guidance on selecting the best microcontroller for my application, that being either the 90 MHz Picollo or 150 MHz Delfino. I've added a bunch of features to the current setup so was looking for the solution that would work and require the least amount of rework by porting over to a new controller.
Any suggestions are appreciated. Thanks,
Troy