Hi,
I am working on creating a labscale microgrid for which I was going through some of your High Volatge Inverter DC-AC kits. I have checked the following products. 1) TMDSHV1PHINVKIT (http://www.ti.com/lit/an/sprabr5/sprabr5.pdf) 2) TI C2000 Solar inverter Kit (http://www.ti.com/lit/ml/sprt615c/sprt615c.pdf) 3) Solar Micro Inverter Development Kit (TMDSSOLARUINVKIT) (http://www.ti.com/lit/an/spraae3/spraae3.pdf) I have certain requirements which are listed below. I would like to have access to: 1) analog signals for all the voltages and currents. (Before and after as well as the inductor current) 2) If I have two such kits, can I use a common clock for both of them (or can the clocks of both the kits be synchronized?) Please let me know which of the kits listed above have the required functionality available.. If these features are not supported by the kits mentioned above, please let me know about any other inverter kit with the required functionality. It would be helpful if I could personally talk to a technical representative about my requirements. Please let me know if it is possible.
Thanks