Hi, Im using C2000 development kit with TMS320F28035 controller to drive ESTUN EMJ-04APB22 AC servomotor with the 2.1 PMSM code in ControlSUITE.
I have some troubles with QEP signals from the encoder. If I power only the controller, the variable RawTheta of the qep1 structure increases its valor while i move the rotor. But if I power the motor, the variable stops to count qep impulses. I think it due to GND potential that oscillates around ground potential of the motor shell.
Did anyone had same problem?