Hi there
My Concerto is working fine running a web page when I use DHCP and a router, so I can connect with the concerto from anywhere in or outside my network.
However, when I connect the Concerto directly to a wall socket with a Static IP (with no router) I only can connect with the Concerto from inside my network (but not from outside).
I've realized that uip doesn't allow setting up a Gateway (only allows Static IP + Subnet Mask) whereas a router using DHCP sends to the Concerto all the configuration (IP+subnet mask+gateway) and this way it works from everywhere inside or outside my network.
Is there any way to define a Gateway in the euip with Static IP?
When using uip with static IP is ti only possible get connection from inside my own network?
Thanks so much.
Dionisio